您好,
客户假设一个理想的3.3V电源,带有0个斜坡。 他使用外部重置器件来监控电源,并在3.3V的情况下对MSP430G2230进行重置。
—他是否可以立即释放复位,或者他是否需要考虑稳定振荡器,MCU上升的延迟,... ?
-内部复位是否始终需要2毫秒的TD (BOR)延迟? 即使电源设备快速上升(0)?
- D/s (第19页)提到V (B_IT–) TYP=1.35V,max=1V。 这是正确的还是应该是TYP=1.35V和MIN=1V?
此致,Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
客户假设一个理想的3.3V电源,带有0个斜坡。 他使用外部重置器件来监控电源,并在3.3V的情况下对MSP430G2230进行重置。
—他是否可以立即释放复位,或者他是否需要考虑稳定振荡器,MCU上升的延迟,... ?
-内部复位是否始终需要2毫秒的TD (BOR)延迟? 即使电源设备快速上升(0)?
- D/s (第19页)提到V (B_IT–) TYP=1.35V,max=1V。 这是正确的还是应该是TYP=1.35V和MIN=1V?
此致,Holger
您好,Holger,
16MHz振荡器在VCC达到3.3V时运行良好,因此外部复位设备可以在检测到VCC稳定在3.3V时立即释放MCU。
MCU默认使用1MHz时钟,并且在振荡器从复位释放后实际设置为16MHz之前,根据其程序的执行速度,会有一些固有的延迟。 有些客户会单独测量其系统的VCC斜坡特性,并在代码中增加额外的内部延迟,以便MCU可以在1MHz时钟的3.3V以下工作,但要等待安全的时间, 为提高时间效率,将振荡器设置为16MHz时,VCC之前的已知时间为3.3V以上。 在MCU振荡器设置为16MHz时,外部重置设备必须确保VCC处于或高于3.3V。
此致,
Ryan