This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP-EXP430FR5994:DMA ISR 有时不会触发

Guru**** 2535750 points
Other Parts Discussed in Thread: MSP-EXP430FR5994, BQ79616

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1115297/msp-exp430fr5994-dma-isr-will-sometimes-not-trigger

器件型号:MSP-EXP430FR5994

我让 MSP-EXP430FR5994通过 UART 与 BQ79600 EVM 通信;DMA 用于 UART 接收。 BQ79600 EVM 连接到定制的 BQ79616 PCB。 通信成功大部分时间、BQ 芯片能够测量电池电压和温度。 我已经通过在 CCS 中启动调试会话来确认这一点、并使用逻辑分析仪捕获5秒的触发。 之后、我停止 CCS 并查看表达式。 附件是成功的 IDE 表达式(BQUartDMASuccesss.PNG)的屏幕截图。

在大约7个这样的 IDE 运行之后、BQ 自动寻址序列在第一个 DLL 丢弃后停止读取。 BQ 芯片正在响应此第一步、如所附的逻辑分析仪屏幕截图(AABREAA.PNG)中所示。 DMA ISR 不会触发。 从随附的 IDE 屏幕截图(dmaRxAA.PNG)中、dma_value 缓冲区正在接收全部7个预期字节。 我想了解 DMA ISR 为什么与触发有关是偶发的。

 

#define BQUART_enableInterrupt        EUSCI_A_UART_enableInterrupt
#define BQUART_RX_INT                 EUSCI_A_UART_RECEIVE_INTERRUPT
#define BQUART_clearInterrupt         EUSCI_A_UART_clearInterrupt
#define BQUART_TXBUF                  UCA1TXBUF
#define BQUART_RXBUF                  UCA1RXBUF
#define BQUART_IFG                    UCA1IFG


#define BQUART_ISR                    USCI_A1_ISR
#define BQUART_VECTOR                 USCI_A1_VECTOR
#define BQUART_IFG                    UCA1IFG
#define BQUART_IV                     UCA1IV


#define BQUART_DMA_RX_TRIGGER         DMA1TSEL__UCA1RXIFG
#define BQUART_DMASA                  DMA1SA
#define BQUART_DMADA                  DMA1DA
#define BQUART_DMAxCTL                DMA1CTL           //DMA Channel 1
#define BQUART_DMACTLx                DMACTL0           //holds the DMA trigger
#define BQUART_DMAIV_IFG              DMAIV_DMA1IFG
#define BQUART_DMASZ                  DMA1SZ

/*
 * uartCommands.c
 *
 *  Created on: Apr 21, 2022
 *      Author: Priya.Nadathur
 */


#include <driverlib.h>
#include <string.h>
#include "bspFuncs.h"
#include "mbbConfig.h"
#include "timer.h"
#include "B0_reg.h"

#ifdef BQ_UART
#include "uartCommands.h"

extern uint16_t bq79600Addr;

extern BYTE autoaddr_response_frame[(1+6)*TOTALBOARDS];
extern uint8_t response_frame[(8)*TOTALBOARDS];

uint8_t uartRxLen;
uint8_t dmaDataReady = 0;
uint16_t dma_value[(8)*TOTALBOARDS] = {0};
uint8_t startMeasure = 0;
uint8_t bqAddr = 0;

// CRC16 TABLE
// ITU_T polynomial: x^16 + x^15 + x^2 + 1
const uint16_t crc16_table[256] = { 0x0000, 0xC0C1, 0xC181, 0x0140, 0xC301,
        0x03C0, 0x0280, 0xC241, 0xC601, 0x06C0, 0x0780, 0xC741, 0x0500, 0xC5C1,
        0xC481, 0x0440, 0xCC01, 0x0CC0, 0x0D80, 0xCD41, 0x0F00, 0xCFC1, 0xCE81,
        0x0E40, 0x0A00, 0xCAC1, 0xCB81, 0x0B40, 0xC901, 0x09C0, 0x0880, 0xC841,
        0xD801, 0x18C0, 0x1980, 0xD941, 0x1B00, 0xDBC1, 0xDA81, 0x1A40, 0x1E00,
        0xDEC1, 0xDF81, 0x1F40, 0xDD01, 0x1DC0, 0x1C80, 0xDC41, 0x1400, 0xD4C1,
        0xD581, 0x1540, 0xD701, 0x17C0, 0x1680, 0xD641, 0xD201, 0x12C0, 0x1380,
        0xD341, 0x1100, 0xD1C1, 0xD081, 0x1040, 0xF001, 0x30C0, 0x3180, 0xF141,
        0x3300, 0xF3C1, 0xF281, 0x3240, 0x3600, 0xF6C1, 0xF781, 0x3740, 0xF501,
        0x35C0, 0x3480, 0xF441, 0x3C00, 0xFCC1, 0xFD81, 0x3D40, 0xFF01, 0x3FC0,
        0x3E80, 0xFE41, 0xFA01, 0x3AC0, 0x3B80, 0xFB41, 0x3900, 0xF9C1, 0xF881,
        0x3840, 0x2800, 0xE8C1, 0xE981, 0x2940, 0xEB01, 0x2BC0, 0x2A80, 0xEA41,
        0xEE01, 0x2EC0, 0x2F80, 0xEF41, 0x2D00, 0xEDC1, 0xEC81, 0x2C40, 0xE401,
        0x24C0, 0x2580, 0xE541, 0x2700, 0xE7C1, 0xE681, 0x2640, 0x2200, 0xE2C1,
        0xE381, 0x2340, 0xE101, 0x21C0, 0x2080, 0xE041, 0xA001, 0x60C0, 0x6180,
        0xA141, 0x6300, 0xA3C1, 0xA281, 0x6240, 0x6600, 0xA6C1, 0xA781, 0x6740,
        0xA501, 0x65C0, 0x6480, 0xA441, 0x6C00, 0xACC1, 0xAD81, 0x6D40, 0xAF01,
        0x6FC0, 0x6E80, 0xAE41, 0xAA01, 0x6AC0, 0x6B80, 0xAB41, 0x6900, 0xA9C1,
        0xA881, 0x6840, 0x7800, 0xB8C1, 0xB981, 0x7940, 0xBB01, 0x7BC0, 0x7A80,
        0xBA41, 0xBE01, 0x7EC0, 0x7F80, 0xBF41, 0x7D00, 0xBDC1, 0xBC81, 0x7C40,
        0xB401, 0x74C0, 0x7580, 0xB541, 0x7700, 0xB7C1, 0xB681, 0x7640, 0x7200,
        0xB2C1, 0xB381, 0x7340, 0xB101, 0x71C0, 0x7080, 0xB041, 0x5000, 0x90C1,
        0x9181, 0x5140, 0x9301, 0x53C0, 0x5280, 0x9241, 0x9601, 0x56C0, 0x5780,
        0x9741, 0x5500, 0x95C1, 0x9481, 0x5440, 0x9C01, 0x5CC0, 0x5D80, 0x9D41,
        0x5F00, 0x9FC1, 0x9E81, 0x5E40, 0x5A00, 0x9AC1, 0x9B81, 0x5B40, 0x9901,
        0x59C0, 0x5880, 0x9841, 0x8801, 0x48C0, 0x4980, 0x8941, 0x4B00, 0x8BC1,
        0x8A81, 0x4A40, 0x4E00, 0x8EC1, 0x8F81, 0x4F40, 0x8D01, 0x4DC0, 0x4C80,
        0x8C41, 0x4400, 0x84C1, 0x8581, 0x4540, 0x8701, 0x47C0, 0x4680, 0x8641,
        0x8201, 0x42C0, 0x4380, 0x8341, 0x4100, 0x81C1, 0x8081, 0x4040 };


BYTE bBuf[8];

uint8_t pFrame[64];
int bRes = 0;
BYTE bReturn = 0;

BYTE* currCRC;
int crc_i = 0;
uint16_t wCRC2 = 0xFFFF;
int crc16_i = 0;

/**
 * @brief Setup DMA for BQ UART receive
 *
 * Single transfer; increment destination address; source address unchanged;
 * byte to word transfer source to DMA; word to byte transfer destination to DMA;
 * rising edge DMA trigger; DMA enable
 *
 */

void DMA_Init(){
    __data20_write_long((uintptr_t)&BQUART_DMASA, (uintptr_t)&BQUART_RXBUF);
    __data20_write_long((uintptr_t)&BQUART_DMADA, (uintptr_t) dma_value);

    BQUART_DMAxCTL &= ~DMAEN;
    BQUART_DMACTLx |= BQUART_DMA_RX_TRIGGER;
    DMACTL4 |= DMARMWDIS;

    BQUART_DMAxCTL |= DMADT_0|DMADSTINCR_3|DMASRCINCR_0|DMASRCBYTE__WORD|DMADSTBYTE__WORD|DMA_TRIGGER_RISINGEDGE|DMAEN;

}

/**
 * @brief Configure BQ UART @1000000 baud
 *
 * software-dl.ti.com/.../index.html
 */

void UART_Init(void){

    BQUART_initParam param = {0};

    param.clockPrescalar = 4,
    param.firstModReg = 0,
    param.secondModReg = 0,
    param.selectClockSource = BQUART_CLOCKSOURCE;
    param.parity =            BQUART_PARITY;
    param.msborLsbFirst =     BQUART_BITORDER;
    param.numberofStopBits =  BQUART_STOPBIT;
    param.uartMode =          BQUART_MODE;
    param.overSampling =      BQUART_OVERSAMPLING;

    if(STATUS_FAIL == BQUART_INIT(BQUART, &param))
    {
       return;
    }

    BQUART_enable(BQUART);
}

//FORMAT WRITE DATA, SEND TO
//BE COMBINED WITH REST OF FRAME

int WriteReg(BYTE bID, uint16_t wAddr, uint64_t dwData, BYTE bLen, BYTE bWriteType){
    // device address, register start address, data bytes, data length, write type (single, broadcast, stack)
    bRes = 0;
    memset(bBuf,0,sizeof(bBuf));
    switch (bLen) {
    case 1:
        bBuf[0] = dwData & 0x00000000000000FF;
        bRes = WriteFrame(bID, wAddr, bBuf, 1, bWriteType);
        break;
    case 2:
        bBuf[0] = (dwData & 0x000000000000FF00) >> 8;
        bBuf[1] = dwData & 0x00000000000000FF;
        bRes = WriteFrame(bID, wAddr, bBuf, 2, bWriteType);
        break;
    case 3:
        bBuf[0] = (dwData & 0x0000000000FF0000) >> 16;
        bBuf[1] = (dwData & 0x000000000000FF00) >> 8;
        bBuf[2] = dwData & 0x00000000000000FF;
        bRes = WriteFrame(bID, wAddr, bBuf, 3, bWriteType);
        break;
    case 4:
        bBuf[0] = (dwData & 0x00000000FF000000) >> 24;
        bBuf[1] = (dwData & 0x0000000000FF0000) >> 16;
        bBuf[2] = (dwData & 0x000000000000FF00) >> 8;
        bBuf[3] = dwData & 0x00000000000000FF;
        bRes = WriteFrame(bID, wAddr, bBuf, 4, bWriteType);
        break;
    case 5:
        bBuf[0] = (dwData & 0x000000FF00000000) >> 32;
        bBuf[1] = (dwData & 0x00000000FF000000) >> 24;
        bBuf[2] = (dwData & 0x0000000000FF0000) >> 16;
        bBuf[3] = (dwData & 0x000000000000FF00) >> 8;
        bBuf[4] = dwData & 0x00000000000000FF;
        bRes = WriteFrame(bID, wAddr, bBuf, 5, bWriteType);
        break;
    case 6:
        bBuf[0] = (dwData & 0x0000FF0000000000) >> 40;
        bBuf[1] = (dwData & 0x000000FF00000000) >> 32;
        bBuf[2] = (dwData & 0x00000000FF000000) >> 24;
        bBuf[3] = (dwData & 0x0000000000FF0000) >> 16;
        bBuf[4] = (dwData & 0x000000000000FF00) >> 8;
        bBuf[5] = dwData & 0x00000000000000FF;
        bRes = WriteFrame(bID, wAddr, bBuf, 6, bWriteType);
        break;
    case 7:
        bBuf[0] = (dwData & 0x00FF000000000000) >> 48;
        bBuf[1] = (dwData & 0x0000FF0000000000) >> 40;
        bBuf[2] = (dwData & 0x000000FF00000000) >> 32;
        bBuf[3] = (dwData & 0x00000000FF000000) >> 24;
        bBuf[4] = (dwData & 0x0000000000FF0000) >> 16;
        bBuf[5] = (dwData & 0x000000000000FF00) >> 8;
        bBuf[6] = dwData & 0x00000000000000FF;
        bRes = WriteFrame(bID, wAddr, bBuf, 7, bWriteType);
        break;
    case 8:
        bBuf[0] = (dwData & 0xFF00000000000000) >> 56;
        bBuf[1] = (dwData & 0x00FF000000000000) >> 48;
        bBuf[2] = (dwData & 0x0000FF0000000000) >> 40;
        bBuf[3] = (dwData & 0x000000FF00000000) >> 32;
        bBuf[4] = (dwData & 0x00000000FF000000) >> 24;
        bBuf[5] = (dwData & 0x0000000000FF0000) >> 16;
        bBuf[6] = (dwData & 0x000000000000FF00) >> 8;
        bBuf[7] = dwData & 0x00000000000000FF;
        bRes = WriteFrame(bID, wAddr, bBuf, 8, bWriteType);
        break;
    default:
        break;
    }
    return bRes;
}

//GENERATE COMMAND FRAME
int WriteFrame(BYTE bID, uint16_t wAddr, BYTE * pData, BYTE bLen, BYTE bWriteType) {
    int bPktLen = 0;
    uint8_t * pBuf = pFrame;
    uint16_t wCRC;
    memset(pFrame, 0x7F, sizeof(pFrame));

    *pBuf++ = 0x80 | (bWriteType) | ((bWriteType & 0x10) ? bLen - 0x01 : 0x00); //Only include blen if it is a write; Writes are 0x90, 0xB0, 0xD0
    if (bWriteType == FRMWRT_SGL_R || bWriteType == FRMWRT_SGL_W)
    {
        *pBuf++ = (bID & 0x00FF);
    }
    *pBuf++ = (wAddr & 0xFF00) >> 8;
    *pBuf++ = wAddr & 0x00FF;

    while (bLen--)
        *pBuf++ = *pData++;

    bPktLen = pBuf - pFrame;

    wCRC = CRC16(pFrame, bPktLen);
    *pBuf++ = wCRC & 0x00FF;
    *pBuf++ = (wCRC & 0xFF00) >> 8;
    bPktLen += 2;
    //THIS SEEMS to occasionally drop bytes from the frame. Sometimes is not sending the last frame of the CRC.
    //(Seems to be caused by stack overflow, so take precautions to reduce stack usage in function calls)
    uartSend(bPktLen, pFrame);

    return bPktLen;
}


//GENERATE READ COMMAND FRAME AND THEN WAIT FOR RESPONSE DATA (INTERRUPT MODE FOR SCIRX)
int ReadReg(BYTE bID, uint16_t wAddr, BYTE * pData, BYTE bLen, uint32_t dwTimeOut, BYTE bWriteType) {
    // device address, register start address, byte frame pointer to store data, data length, read type (single, broadcast, stack)
    int crcChk;
    bRes = 0;

    if (bWriteType == FRMWRT_SGL_R) {
        ReadFrameReq(bID, wAddr, bLen, bWriteType, bLen+6);
        memset(pData, 0, sizeof(pData));


    } else if (bWriteType == FRMWRT_STK_R) {
        bRes = ReadFrameReq(bID, wAddr, bLen, bWriteType, (bLen + 6) * (TOTALBOARDS - 1));
        memset(pData, 0, sizeof(pData));

    } else if (bWriteType == FRMWRT_ALL_R) {
        bRes = ReadFrameReq(bID, wAddr, bLen, bWriteType, (bLen + 6) * TOTALBOARDS);
        memset(pData, 0, sizeof(pData));

    } else {
        bRes = 0;
    }

//    //CHECK IF CRC IS CORRECT
    for(crc_i=0; crc_i<bRes; crc_i+=(bLen+6))
    {
        if(CRC16(&pData[crc_i], bLen+6)!=0)
        {
//            printConsole("\n\rBAD CRC=%04X,i=%d,bLen=%d\n\r",(pData[crc_i+bLen+4]<<8|pData[crc_i+bLen+5]),crc_i,bLen);
//            PrintFrame(pData, bLen);
            crcChk = 1;
        }
        else crcChk = 0;
    }
    /*
    crc_i = 0;
    currCRC = pData;
    for(crc_i=0; crc_i<bRes; crc_i+=(bLen+6))
    {
        printConsole("%x",&currCRC);
        if(CRC16(currCRC, bLen+6)!=0)
        {
            printConsole("BAD CRC=%04X,byte=%d\n\r",(currCRC[bLen+4]<<8|currCRC[bLen+5]),crc_i);
            PrintFrame(pData, bLen);
        }
       *currCRC+=(bLen+6);
    }
*/
    return crcChk;
}


int ReadFrameReq(BYTE bID, uint16_t wAddr, BYTE bByteToReturn, BYTE bWriteType, BYTE rxLen) {
    bReturn = bByteToReturn - 1;

    uartRxLen = rxLen;

    //PN setting a flag to identify when BQ79600 address is being read
    if (wAddr == 0x2001)
        bqAddr = 1;

    if (bReturn > 127)
        return 0;

    return WriteFrame(bID, wAddr, &bReturn, 1, bWriteType);
}
uint16_t CRC16(BYTE *pBuf, int nLen) {
    wCRC2 = 0xFFFF;
    //printConsole("CRCOUT = \t");
    for (crc16_i = 0; crc16_i < nLen; crc16_i++) {
        //printConsole("%02x ",*pBuf);
        wCRC2 ^= (*pBuf++) & 0x00FF;
        wCRC2 = crc16_table[wCRC2 & 0x00FF] ^ (wCRC2 >> 8);
    }
    //printConsole("\n\r");

    return wCRC2;
}

/**
 * @brief MSP430 UART transmit data
 *
 * Enable DMA transfer for UART receive and transmit UART data
 *
 * @param[in] transmit packet length
 *            data to transmit
 */
void uartSend(int length, uint8_t * data){
    uint8_t i;

    BQUART_DMASZ = uartRxLen;
    dmaDataReady = 0;
    BQUART_IFG &= ~UCRXIFG;     //clear UART receive buffer

    BQUART_DMAxCTL |= DMAEN;
    BQUART_DMAxCTL |= DMAIE;


    for (i = 0; i < length; i++){
        while (!(BQUART_IFG & UCTXIFG));
        BQUART_TXBUF = data[i];
    }


}

/**
 * @brief Receive MSP430 UART
 *
 * After DMA receive transfer is complete, copy the data over to BQ data processing arrays
 */
void uartReceive(void){
uint8_t i;

   if (startMeasure == 1){
       for (i = 0; i < uartRxLen; i++){
          response_frame[i] = dma_value[i];
       }
       dmaDataReady = 1;
   }

   if (bq79600Addr != Bridge_DEV_CONF1_Response){
       for (i = 0; i < uartRxLen; i++){
          autoaddr_response_frame[i] = dma_value[i];
       }
       dmaDataReady = 1;
       bq79600Addr = autoaddr_response_frame[4];
   }

}

/**
 * @brief DMA ISR: BQUART_DMA_RX_TRIGGER
 */
#pragma vector=DMA_VECTOR
__interrupt void dmaIsrHandler(void)
{
    switch(__even_in_range(DMAIV,  BQUART_DMAIV_IFG))
    {
    case BQUART_DMAIV_IFG:
        BQUART_DMAxCTL &= ~DMAIE;

        uartReceive();

        // Exit low power mode on wake-up
        __bic_SR_register_on_exit(LPM4_bits);
        break;
    case DMAIV_DMA0IFG:
        break;

    case DMAIV_DMA2IFG:
        break;

    case DMAIV_DMA3IFG:
            break;

    case DMAIV_DMA4IFG:
        break;

    case DMAIV_DMA5IFG:
        break;

    default: break;
    }
}

#endif

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果调试会话仍处于打开状态、请发布 DMA1寄存器的内容("Registers"视图)。 DMA1SZ 和(通常) DMA1CTL 通常提供一些线索来了解发生了什么。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    当 AA 序列不进行时、我将在完成5秒触发后捕获寄存器内容。 当情况不起作用时、寄存器显示 DMA1SZ=1。 不确定原因、变量 uartRxLen 正在读取正确数量的字节、即7。 (显示在第一个帖子 dmaRxAA 的屏幕截图中)。 当工作正常时、我还附加了 DMA 寄存器内容。

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我需要一些有关后续步骤的指示、或者这里可能会有什么问题。 我不知道 DMA 寄存器如何具有与分配给它的正确值的变量不同的值。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    如果知道 SZ=1、就会消除许多可能的解释。  

    接下来我要做的是:

    1) 1)检查 UART 状态(UCA1STATW)是否存在传输错误、尤其是帧(FE)或溢出(OE)、以查看丢失字节的位置。

    2) 2)在启动 DMA 之前、尝试清除 dma_values[]缓冲区(或至少清除 dma_values[6])、以确保不会看到上一个操作的剩余内容。

    3) 3)恰好在 uartSend 中设置 DMAEN 之前、尝试先清除 DMAEN。 这将在发生竞争时重置通道。

    4) 4)如果可以、请考虑加快 CPU (MCLK)速度、这将使 DMA 相对于串行端口的运行速度更快。    DMA 不能跟上足够快的源代码是异常的、但可能的。 (这与上面的(1)有关。)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢你的答复。 无 UART 发送错误。 MCU 已以最大时钟16MHz 运行。  

    我尝试了建议2和3、他们似乎对问题有所帮助。 通过10次从 CCS 启动 BQ 固件的试验、BQ 初始化和测量成功。 我重复了10次试验、只是为了确保。 问题现已解决。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我很高兴您能正常工作。

    如果步骤(3)确实修复了某个问题、这表明此处存在一些对于普通读者而言不明显的流程。 保持 DMAEN 切换("廉价保险")、但留意其他古怪的东西。 (除了 DMA ISR 之外、您还有多个唤醒源吗?)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    固件中有一个每125ms 生成一个 ISR 的主计时器。 这是唯一的其他 ISR。 我可以在启动 DMA 传输并重新启用它之前禁用它。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    只需清除:通过唤醒、我指的是"BIC_SR_REGISTER_ON_EXIT (LPMx_Bits)"、而不仅仅是任何 ISR。  

    危险(正如您所猜测的)是 LPM 受到源 A 的影响、但代码假定它是源 B、并且东西会变得混乱。 在停止"心跳"计时器的过程中、可能有一种消除(状态变量或其他内容)歧义的方法、但也可能值得一试(因为此时您非常接近问题)。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    MSP430何时进入 LPM? LPM 中的电流消耗非常低、但我想知道 MSP430在 LPM 中保持多长时间?

    您能否举例说明您所说的状态变量?

    LPM4_BITS 目前是 SCG1+SCG0+OSCOFF+CPUOFF --是否要添加到此列表中?

    删除  _BIC_SR_REGISTER_ON_EXIT (LPM4_BITS)是否有助于解决此问题?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    使用类似于"_Bis_SR_register (LPMx_bits)"的内容来输入 LPM。

    我没有看到您的 main()程序,因此我不知道它的作用。 当我在 DMA ISR 中看到唤醒代码时、我本来应该使用 LPM、但听起来可能根本没有。 如果不去 LPM (睡眠)、唤醒不做任何事情(也不会伤害任何东西)。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我在 main.c 中没有任何内容可用于输入 LPM。 我将删除 __BIC_SR_REGISTER_ON_EXIT (LPM4_BITS);

    谢谢