This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR2475:双通道 UART 不工作

Guru**** 2524550 points
Other Parts Discussed in Thread: MSP430FR2475

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1057066/msp430fr2475-dual-channel-uart-not-working

器件型号:MSP430FR2475

大家好!!

我正在尝试在 MSP430FR2475中使用两个 UART 通道、我已成功实现具有接收中断的 UART1 (115200波特率)、 但现在我正在尝试以相同的波特率实现具有接收中断的 UART0、但它不起作用。AM 遵循 UART1针对 UART0的相同程序、有什么问题? 我已经提到下面的代码、请检查、如果您有解决方案、请提前通知我、谢谢。

int main(void)
{
        Clock_Init();
        GPIO_Init();
        UART1_Init();
        UART0_Init();
        Software_Trim();
       UCA0TXBUF =30;(Not Working)
       while(!(UCA0IFG&UCTXIFG));
       _delay_cycles(500);
       UCA1TXBUF =20;(Working)
       while(!(UCA1IFG&UCTXIFG));
       _delay_cycles(500);
        while(1)
        {
        }
}
#pragma vector=USCI_A1_VECTOR// Sensor ( Working UART)
__interrupt void USCI_A1_ISR(void)
{
    UCA1IFG &=~ UCRXIFG;
    rx_buffer[rx_ptr++] = UCA1RXBUF;
}
//UART master
#pragma vector=USCI_A0_VECTOR (Not Working UART)
__interrupt void USCI_A0_ISR(void)
{
    UCA0IFG &=~ UCRXIFG;
    m_rx_buffer[m_rx_ptr++] = UCA0RXBUF;

}

void GPIO_Init(void)
{
        P3DIR |= BIT7;
        P3DIR|= BIT5; //RX Encoder
        P3DIR &= ~BIT7;
        //P5DIR &= ~ BIT0;//Master enable
        P2DIR |=  BIT4;//LMS enable
        P5DIR |=  BIT0;//master enable
}


void UART0_Init()//Master
{
    SYSCFG3 |= USCIA0RMP;   //eUSCI_A port remap
    P5SEL0 |= BIT1 | BIT2;

    UCA0CTLW0 |= UCSWRST;
    UCA0CTLW0 |= UCSSEL__SMCLK;
    UCA0CTLW0 |= UCPEN_1 | UCPAR__EVEN;
    UCA0BR0 = 4; // 9600 baud rate
    UCA0BR1 = 0x00;
    UCA0MCTLW = 0x4900 | UCOS16 | UCBRF_5;

    UCA0CTLW0 &= ~UCSWRST;                    // Initialize eUSCI
    UCA0IE |= UCRXIE;                         // Enable USCI_A1 RX interrupt
  
    __bis_SR_register(GIE);
}

void UART1_Init()//LMS OKAY
{
    SYSCFG3 |= USCIA0RMP;   //eUSCI_A port remap
    P2SEL0 |= BIT5 | BIT6;
     UCA1CTLW0 |= UCSWRST;
     UCA1CTLW0 |= UCSSEL__SMCLK;
     UCA1CTLW0 |= UCPEN_1 | UCPAR__EVEN;
    UCA1BR0 = 4;                             // 8000000/16/115200
    UCA1BR1 = 0x00;
     UCA1MCTLW = 0x4900 | UCOS16 | UCBRF_5;
     UCA1CTLW0 &= ~UCSWRST;                    // Initialize eUSCI
     UCA1IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
     __bis_SR_register(GIE);         // interrupts enabled

}




void Clock_Init(void)
{
       WDTCTL = WDTPW | WDTHOLD;               // Stop watchdog timer
       __bis_SR_register(SCG0);                // disable FLL
       CSCTL3 |= SELREF__REFOCLK;              // Set REFO as FLL reference source
       CSCTL1 = DCOFTRIMEN_1 | DCOFTRIM0 | DCOFTRIM1 | DCORSEL_3;// DCOFTRIM=3, DCO Range = 8MHz
       CSCTL2 = FLLD_0 + 243;                  // DCODIV = 8MHz
       __delay_cycles(3);
       __bic_SR_register(SCG0);                // enable FLL
       Software_Trim();                         // Software Trim to get the best DCOFTRIM value
       PM5CTL0 &= ~LOCKLPM5;                   // Disable the GPIO power-on default high-impedance mode
                                               // to activate previously configured port settings
       }

void Software_Trim()
{
    unsigned int oldDcoTap = 0xffff;
    unsigned int newDcoTap = 0xffff;
    unsigned int newDcoDelta = 0xffff;
    unsigned int bestDcoDelta = 0xffff;
    unsigned int csCtl0Copy = 0;
    unsigned int csCtl1Copy = 0;
    unsigned int csCtl0Read = 0;
    unsigned int csCtl1Read = 0;
    unsigned int dcoFreqTrim = 3;
    unsigned char endLoop = 0;

    do
    {
        CSCTL0 = 0x100;                         // DCO Tap = 256
        do
        {
            CSCTL7 &= ~DCOFFG;                  // Clear DCO fault flag
        }while (CSCTL7 & DCOFFG);               // Test DCO fault flag

        __delay_cycles((unsigned int)3000 * MCLK_FREQ_MHZ);// Wait FLL lock  (FLLUNLOCK) to be stable
                                                           // Suggest to wait 24 cycles of divided FLL reference clock
        while((CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)) && ((CSCTL7 & DCOFFG) == 0));

        csCtl0Read = CSCTL0;                   // Read CSCTL0
        csCtl1Read = CSCTL1;                   // Read CSCTL1

        oldDcoTap = newDcoTap;                 // Record DCOTAP value of last time
        newDcoTap = csCtl0Read & 0x01ff;       // Get DCOTAP value of this time
        dcoFreqTrim = (csCtl1Read & 0x0070)>>4;// Get DCOFTRIM value

        if(newDcoTap < 256)                    // DCOTAP < 256
        {
            newDcoDelta = 256 - newDcoTap;     // Delta value between DCPTAP and 256
            if((oldDcoTap != 0xffff) && (oldDcoTap >= 256)) // DCOTAP cross 256
                endLoop = 1;                   // Stop while loop
            else
            {
                dcoFreqTrim--;
                CSCTL1 = (csCtl1Read & (~DCOFTRIM)) | (dcoFreqTrim<<4);
            }
        }
        else                                   // DCOTAP >= 256
        {
            newDcoDelta = newDcoTap - 256;     // Delta value between DCPTAP and 256
            if(oldDcoTap < 256)                // DCOTAP cross 256
                endLoop = 1;                   // Stop while loop
            else
            {
                dcoFreqTrim++;
                CSCTL1 = (csCtl1Read & (~DCOFTRIM)) | (dcoFreqTrim<<4);
            }
        }

        if(newDcoDelta < bestDcoDelta)         // Record DCOTAP closest to 256
        {
            csCtl0Copy = csCtl0Read;
            csCtl1Copy = csCtl1Read;
            bestDcoDelta = newDcoDelta;
        }

    }while(endLoop == 0);                      // Poll until endLoop == 1

    CSCTL0 = csCtl0Copy;                       // Reload locked DCOTAP
    CSCTL1 = csCtl1Copy;                       // Reload locked DCOFTRIM
    while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
}

此致、

Aravinth K

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您能否阻止所有 UART1代码并保留 UART0并对其进行测试?  

    此致、

    现金 Hao

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您如何判断它不起作用? 更广泛地说:您使用的是什么电路板、它是如何布线的? (我不知道用于 FR2475的任何商业分线板。)

    我将此代码放置在交叉连接 UCA0+UCA1的 FR2476 Launchpad 上、我看到每个 RX_buffer-s 中存储了一个字节(20/30) 我希望我们能做 不同的事情。