This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP-EXP430G2ET:与 TMP1075EVM 的 I2C 接口

Guru**** 2686715 points

Other Parts Discussed in Thread: TMP1075, MSP430FR2433

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1023899/msp-exp430g2et-i2c-interface-with-the-tmp1075evm

器件型号:MSP-EXP430G2ET
主题中讨论的其他器件:TMP1075MSP430FR2433

您好!

我目前正在尝试通过 I2C 通信将 MSP430G2ET 连接到 TMP1075。 下面是我在 Code Composer Studio 中使用的代码以及我看到的输出、根据我的理解、我必须更正 TMP1075的地址、但当我尝试读取"接收缓冲器值时、我只看到0x00。 我应该读取另一个值吗?我通过 I2C 进行通信的方式是否有问题?

//******************************************************************************
//   MSP430G2xx3 Demo - USCI_B0, I2C Master multiple byte TX/RX
//
//   Description: I2C master communicates to I2C slave sending and receiving
//   3 different messages of different length. I2C master will enter LPM0 mode
//   while waiting for the messages to be sent/receiving using I2C interrupt.
//   ACLK = NA, MCLK = SMCLK = DCO 16MHz.
//
//
//                   MSP430G2553         3.3V
//                 -----------------   /|\ /|\
//            /|\ |                 |   |  4.7k
//             |  |                 |  4.7k |
//             ---|RST              |   |   |
//                |                 |   |   |
//                |             P1.6|---|---+- I2C Clock (UCB0SCL)
//                |                 |   |
//                |             P1.7|---+----- I2C Data (UCB0SDA)
//                |                 |
//                |                 |
//
//   Nima Eskandari
//   Texas Instruments Inc.
//   April 2017
//   Built with CCS V7.0
//******************************************************************************

#include <msp430.h>
#include <stdint.h>
#include <stdbool.h>

//******************************************************************************
// Example Commands ************************************************************
//******************************************************************************

#define SLAVE_ADDR  0x48
#define CONVERSION_READY    0x10

/* CMD_TYPE_X_SLAVE are example commands the master sends to the slave.
 * The slave will send example SlaveTypeX buffers in response.
 *
 * CMD_TYPE_X_MASTER are example commands the master sends to the slave.
 * The slave will initialize itself to receive MasterTypeX example buffers.
 * */

#define CMD_TYPE_0_SLAVE      0
#define CMD_TYPE_1_SLAVE      1
#define CMD_TYPE_2_SLAVE      2

#define CMD_TYPE_0_MASTER      3
#define CMD_TYPE_1_MASTER      4
#define CMD_TYPE_2_MASTER      5

#define TYPE_0_LENGTH   1
#define TYPE_1_LENGTH   2
#define TYPE_2_LENGTH   6

#define MAX_BUFFER_SIZE     20

/* MasterTypeX are example buffers initialized in the master, they will be
 * sent by the master to the slave.
 * SlaveTypeX are example buffers initialized in the slave, they will be
 * sent by the slave to the master.
 * */

uint8_t MasterType2 [TYPE_2_LENGTH] = {'F', '4', '1', '9', '2', 'B'};
//uint8_t MasterType1 [TYPE_1_LENGTH] = { 8, 9};
uint8_t MasterType1 [TYPE_1_LENGTH] = { 0x00, 0xFF};
uint8_t MasterType0 [TYPE_0_LENGTH] = { 11};


uint8_t SlaveType2 [TYPE_2_LENGTH] = {0};
uint8_t SlaveType1 [TYPE_1_LENGTH] = {0};
uint8_t SlaveType0 [TYPE_0_LENGTH] = {0};

//******************************************************************************
// General I2C State Machine ***************************************************
//******************************************************************************


typedef enum I2C_ModeEnum{
    IDLE_MODE,
    NACK_MODE,
    TX_REG_ADDRESS_MODE,
    RX_REG_ADDRESS_MODE,
    TX_DATA_MODE,
    RX_DATA_MODE,
    SWITCH_TO_RX_MODE,
    SWITHC_TO_TX_MODE,
    TIMEOUT_MODE
} I2C_Mode;


/* Used to track the state of the software state machine*/
I2C_Mode MasterMode = IDLE_MODE;

/* The Register Address/Command to use*/
uint8_t TransmitRegAddr = 0;

/* ReceiveBuffer: Buffer used to receive data in the ISR
 * RXByteCtr: Number of bytes left to receive
 * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer
 * TransmitBuffer: Buffer used to transmit data in the ISR
 * TXByteCtr: Number of bytes left to transfer
 * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer
 * */
uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t RXByteCtr = 0;
uint8_t ReceiveIndex = 0;
uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0};
uint8_t TXByteCtr = 0;
uint8_t TransmitIndex = 0;



/* I2C Write and Read Functions */

/* For slave device with dev_addr, writes the data specified in *reg_data
 *
 * dev_addr: The slave device address.
 *           Example: SLAVE_ADDR
 * reg_addr: The register or command to send to the slave.
 *           Example: CMD_TYPE_0_MASTER
 * *reg_data: The buffer to write
 *           Example: MasterType0
 * count: The length of *reg_data
 *           Example: TYPE_0_LENGTH
 *  */
I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count);

/* For slave device with dev_addr, read the data specified in slaves reg_addr.
 * The received data is available in ReceiveBuffer
 *
 * dev_addr: The slave device address.
 *           Example: SLAVE_ADDR
 * reg_addr: The register or command to send to the slave.
 *           Example: CMD_TYPE_0_SLAVE
 * count: The length of data to read
 *           Example: TYPE_0_LENGTH
 *  */
I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t count);
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count);


I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t count)
{
    /* Initialize state machine */
    MasterMode = TX_REG_ADDRESS_MODE;
    TransmitRegAddr = reg_addr;
    RXByteCtr = count;
    TXByteCtr = 0;
    ReceiveIndex = 0;
    TransmitIndex = 0;

    /* Initialize slave address and interrupts */
    UCB0I2CSA = dev_addr;
    IFG2 &= ~(UCB0TXIFG + UCB0RXIFG);       // Clear any pending interrupts
    IE2 &= ~UCB0RXIE;                       // Disable RX interrupt
    IE2 |= UCB0TXIE;                        // Enable TX interrupt

    UCB0CTL1 |= UCTR + UCTXSTT;             // I2C TX, start condition
    __bis_SR_register(CPUOFF + GIE);              // Enter LPM0 w/ interrupts

    return MasterMode;

}


I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
    /* Initialize state machine */
    MasterMode = TX_REG_ADDRESS_MODE;
    TransmitRegAddr = reg_addr;

    //Copy register data to TransmitBuffer
    CopyArray(reg_data, TransmitBuffer, count);

    TXByteCtr = count;
    RXByteCtr = 0;
    ReceiveIndex = 0;
    TransmitIndex = 0;

    /* Initialize slave address and interrupts */
    UCB0I2CSA = dev_addr;
    IFG2 &= ~(UCB0TXIFG + UCB0RXIFG);       // Clear any pending interrupts
    IE2 &= ~UCB0RXIE;                       // Disable RX interrupt
    IE2 |= UCB0TXIE;                        // Enable TX interrupt

    UCB0CTL1 |= UCTR + UCTXSTT;             // I2C TX, start condition
    __bis_SR_register(CPUOFF + GIE);              // Enter LPM0 w/ interrupts

    return MasterMode;
}


void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
    uint8_t copyIndex = 0;
    for (copyIndex = 0; copyIndex < count; copyIndex++)
    {
        dest[copyIndex] = source[copyIndex];
    }
}



//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************


void initClockTo16MHz()
{
    if (CALBC1_16MHZ==0xFF)                  // If calibration constant erased
    {
        while(1);                               // do not load, trap CPU!!
    }
    DCOCTL = 0;                               // Select lowest DCOx and MODx settings
    BCSCTL1 = CALBC1_16MHZ;                    // Set DCO
    DCOCTL = CALDCO_16MHZ;
}

void initGPIO()
{
    P1DIR |= BIT0 + BIT1 + BIT2 + BIT3 + BIT4;
    P1OUT &= ~(BIT0 + BIT1 + BIT2 + BIT3 + BIT4);

    P1SEL |= BIT6 + BIT7;                     // Assign I2C pins to USCI_B0
    P1SEL2|= BIT6 + BIT7;                     // Assign I2C pins to USCI_B0
}

void initI2C()
{
    UCB0CTL1 |= UCSWRST;                      // Enable SW reset
    UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;     // I2C Master, synchronous mode
    UCB0CTL1 = UCSSEL_2 + UCSWRST;            // Use SMCLK, keep SW reset
    UCB0BR0 = 160;                            // fSCL = SMCLK/160 = ~100kHz
    UCB0BR1 = 0;
    UCB0I2CSA = SLAVE_ADDR;                   // Slave Address
    UCB0CTL1 &= ~UCSWRST;                     // Clear SW reset, resume operation
    UCB0I2CIE |= UCNACKIE;
}


//******************************************************************************
// Main ************************************************************************
// Send and receive three messages containing the example commands *************
//******************************************************************************

int main(void) {
    WDTCTL = WDTPW | WDTHOLD;    // Stop watchdog timer
    initClockTo16MHz();
    initGPIO();
    initI2C();

    I2C_Master_WriteReg(SLAVE_ADDR, 0x01, MasterType1, TYPE_1_LENGTH);
    while(1)
    {
        // poll every 100ms to see when data is available
        _delay_cycles(1600000);

        I2C_Master_ReadReg(SLAVE_ADDR, 0x00, TYPE_1_LENGTH);
        CopyArray(ReceiveBuffer, SlaveType1, TYPE_1_LENGTH);

        // Check status of conversion ready bit
        if(ReceiveBuffer[1] & CONVERSION_READY)
        {
            I2C_Master_ReadReg(SLAVE_ADDR, 0x00, TYPE_1_LENGTH);
            CopyArray(ReceiveBuffer, SlaveType1, TYPE_1_LENGTH);

            // Set break point here to examine results
            _no_operation();
        }
    }
}


//******************************************************************************
// I2C Interrupt For Received and Transmitted Data******************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCIAB0TX_VECTOR))) USCIAB0TX_ISR (void)
#else
#error Compiler not supported!
#endif
{
  if (IFG2 & UCB0RXIFG)                 // Receive Data Interrupt
  {
      //Must read from UCB0RXBUF
      uint8_t rx_val = UCB0RXBUF;

      if (RXByteCtr)
      {
          ReceiveBuffer[ReceiveIndex++] = rx_val;
          RXByteCtr--;
      }

      if (RXByteCtr == 1)
      {
          UCB0CTL1 |= UCTXSTP;
      }
      else if (RXByteCtr == 0)
      {
          IE2 &= ~UCB0RXIE;
          MasterMode = IDLE_MODE;
          __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
      }
  }
  else if (IFG2 & UCB0TXIFG)            // Transmit Data Interrupt
  {
      switch (MasterMode)
      {
          case TX_REG_ADDRESS_MODE:
              UCB0TXBUF = TransmitRegAddr;
              if (RXByteCtr)
                  MasterMode = SWITCH_TO_RX_MODE;   // Need to start receiving now
              else
                  MasterMode = TX_DATA_MODE;        // Continue to transmision with the data in Transmit Buffer
              break;

          case SWITCH_TO_RX_MODE:
              IE2 |= UCB0RXIE;              // Enable RX interrupt
              IE2 &= ~UCB0TXIE;             // Disable TX interrupt
              UCB0CTL1 &= ~UCTR;            // Switch to receiver
              MasterMode = RX_DATA_MODE;    // State state is to receive data
              UCB0CTL1 |= UCTXSTT;          // Send repeated start
              if (RXByteCtr == 1)
              {
                  //Must send stop since this is the N-1 byte
                  while((UCB0CTL1 & UCTXSTT));
                  UCB0CTL1 |= UCTXSTP;      // Send stop condition
              }
              break;

          case TX_DATA_MODE:
              if (TXByteCtr)
              {
                  UCB0TXBUF = TransmitBuffer[TransmitIndex++];
                  TXByteCtr--;
              }
              else
              {
                  //Done with transmission
                  UCB0CTL1 |= UCTXSTP;     // Send stop condition
                  MasterMode = IDLE_MODE;
                  IE2 &= ~UCB0TXIE;                       // disable TX interrupt
                  __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
              }
              break;

          default:
              __no_operation();
              break;
      }
  }
}


//******************************************************************************
// I2C Interrupt For Start, Restart, Nack, Stop ********************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCIAB0RX_VECTOR
__interrupt void USCIAB0RX_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCIAB0RX_VECTOR))) USCIAB0RX_ISR (void)
#else
#error Compiler not supported!
#endif
{
    if (UCB0STAT & UCNACKIFG)
    {
        UCB0STAT &= ~UCNACKIFG;             // Clear NACK Flags
    }
    if (UCB0STAT & UCSTPIFG)                        //Stop or NACK Interrupt
    {
        UCB0STAT &=
            ~(UCSTTIFG + UCSTPIFG + UCNACKIFG);     //Clear START/STOP/NACK Flags
    }
    if (UCB0STAT & UCSTTIFG)
    {
        UCB0STAT &= ~(UCSTTIFG);                    //Clear START Flags
    }
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    大家好、Thomas、

    我将查看以下资源、以帮助调试您的 I2C 问题。 USCI 和 eUSCI 串行通信的常见解决方案。   

    I2C 最常见的问题是线路上的上拉值不正确、但上面的文档也将帮助您解决其他常见问题。  

    另请 查看我们的 I2C MSP Academy。 这也将有助于您实现连接。 任务3应该对您特别感兴趣。

    https://dev.ti.com/tirex/explore/node?node=ANn42uDC4eb.Ph7o71nKTg__IOGqZri__LATEST

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Jace、

    当在 MSP430G2ET EVM 上使用 I2C 通信协议时、即使在 EVM 上也需要外部上拉电阻器吗?

    谢谢、

    Thomas

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的、大多数 LaunchPad 板上没有 I2C 上拉电阻器、因为引脚具有可能不需要上拉的替代功能。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Jace、  

    我添加了上拉电阻器、但我只能读取一些不接近我要查找的 TMP1075的值。 您对如何进行调试有什么建议吗?

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    根据数据表(SBOS854D)表1、0x179大约为23.5C。 这与环境有很大不同吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我在第一次答复中提到的资源可以帮助进一步调试。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Bruce、您是如何获得0x179的?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您的屏幕截图显示了字节[0、1]=(0x17、0x90)。 低位4位(始终)为0、因此先连接 MSB 会给出0x179[0]。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Bruce、

    感谢您的回答、是否可以判断我是否在不断读取温度值、或者每次运行程序时它是否只有一个值?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    0x179[0]似乎是一个不太可能的"魔术常量":正在读取。

    您可以尝试将手指放在传感器上、以查看它是否测量到不同的温度。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Bruce、

    我尝试过这种方法、Debug 中的"Expressions"选项卡中没有实时更改。 如果我不断点击"Play"和"Pause"、它确实会更改值、但我看不到值的实时更新。 这是因为调试正在分解代码、还是有更好的方法读取寄存器值?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Thomas、

    您在这里轮询温度传感器的频率如何? 温度传感器通常需要一段时间才能看到温度变化、这是因为热量传输相对于 MCU 运行速度而言相对较慢。 在每秒轮询一次以上时、您可能不会看到温度读数发生显著变化。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我每100ms 轮询一次、但当我打开寄存器映射时、我确实看到了刷新寄存器映射时的值变化。 您是否有任何资源可用于存储此信息?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    对于大多数温度读数而言、这似乎太频繁了、除非您仅在短窗口中这样做、并获得与家庭温度计应用类似的平均值。  

    由于您使用的是基于闪存的器件、因此我会通过 RAM 中的数组尽可能多地存储数据、然后如果您想存储数据、将其存储到闪存区域中。 请参阅此器件的闪存写入示例 :https://dev.ti.com/tirex/explore/node?node=AN8U7Pen0Nar.8oONLOGRQ__IOGqZri__LATEST  

    如果您使用的是 FRAM、则只需将数据日志信息直接发送到 FRAM 即可。 有关示例、请参阅 MSP430FR2433 Launchpad 开箱即用体验。  https://dev.ti.com/tirex/explore/node?node=APklmqiHLxlaXk4KngZ-fw__IOGqZri__LATEST

    视频: https://www.youtube.com/watch?v=uDHKeWEMamk