This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] MSP430FR6989:使用 DSPLib.h 进行 FFT 分析

Guru**** 2509855 points
Other Parts Discussed in Thread: MSP430FR6989

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1128408/msp430fr6989-fft-analysis-using-dsplib-h

器件型号:MSP430FR6989

您好!

我使用的是 MSP430FR6989和 BMI160 IMU (Sensors BoosterPack)。 它们通过 I2C 进行通信。 我正在测量 Z 轴加速度、并尝试对接收到的数据执行 FFT。 我有一个以3.5Hz 频率振动的测试平台。 我将使用 DSPLIB.h 中的 FFT 函数 FFT 完成后、我将获取幅值最小时的前5个 FFT 值并将其显示在终端上、但我始终会获得随机频率值。 由于我不是 FFT 算法方面的专家、我不确定我做了什么错误。 如果有人能就如何解决这个问题提出一些建议、我将不胜感激。

谢谢你。

以下是我的代码:

 

#include <msp430.h> 
#include "driverlib.h"
#include "DSPLib.h"
#include <gpio.h>
#include <intrinsics.h>
#include <msp430fr5xx_6xxgeneric.h>
#include <stdint.h>
#include <stdio.h>

//new
//#include "myClocks.h"
//new

//******************************************************************************
// Defines *********************************************************************
//******************************************************************************
//Address if the BMI160
#define SLAVE_ADDR 0x69
//Maximum I2C buffer size
#define MAX_BUFFER_SIZE 20

//Number of FFT samples
#define SAMPLES 4096

/* Declare as persistent to move variable from RAM to FRAM */
#pragma PERSISTENT(input)
int16_t input[SAMPLES] = {0}; //Store samples

#pragma PERSISTENT(max)
int16_t max[SAMPLES] = {0}; //Store frequencies with maximum amplitudes

#pragma PERSISTENT(amp)
int16_t amp[SAMPLES] = {0}; //Store the maximum amplitudes

/* Temporary data array for processing */
DSPLIB_DATA(temp,4)
/* Declare as persistent to move variable to FRAM */
#pragma PERSISTENT(temp)
int16_t temp[3*SAMPLES/2] = {0};

//Global flags for sensor interrupts to avoid interrupt nesting
volatile int motion_trigger = 0;

/* Benchmark cycle counts */
volatile uint32_t cycleCount;



//new

#define UP              0x0010                          // Timer_A Up mode
#define CONTINUOUS      0x0020                          // Timer_A Continuous mode
#define ACLK            0x0100                          // Timer_A SMCLK source
#define DEVELOPMENT     0x5A80                          // Stop the watchdog timer
#define BOUNCE_DELAY    0xA000                          // Delay for Button Bounce
#define MS_10           400                             // Approximate value to count for 10ms
#define SMCLK           0x0200                          // Timer_A SMCLK source



//new



//******************************************************************************
// Frequency Functions *********************************************************
//******************************************************************************

void bubbleSort(int amp[], int max[], int n)
{
   int i, j, temp;
   for (i = 0; i < n-1; i++)
   {
       // Last i elements are already in place
       for (j = 0; j < n-i-1; j++)
       {
           if (amp[j] < amp[j+1])
           {
              temp = max[j];
              max[j] = max[j+1];
              max[j+1] = temp;

              temp = amp[j];
              amp[j] = amp[j+1];
              amp[j+1] = temp;
           }
       }
   }
}

void getMaximums(int16_t input[], int samples, int16_t max[], int16_t amp[])
{
    int i,j = 0;
    for(i=1; i<samples-1; i++)
        {
            if((input[i-1] < input[i]) && (input[i] > input[i+1]))
            {
                amp[j] = input[i];
                max[j++] = i;
            }
        }
    bubbleSort(amp, max, samples);
}

//******************************************************************************
// Timer Functions *************************************************************
//******************************************************************************

int delay(int count)
{
    if(TA1CTL & TAIFG)                                  // If Timer_1 is done counting
    {
        count = count-1;                                        // Decrement count
        TA1CTL = TA1CTL & (~TAIFG);                             // Reset Timer_1
    }
    return count;                                       // Return the value of count
} // end delay
//******************************************************************************
// UART Functions **************************************************************
//******************************************************************************
void UART_transmitString( char *pStr ) //Transmits a string over UART0
{
    while( *pStr )
    {
        while(!(UCA0IFG&UCTXIFG));
        UCA0TXBUF = *pStr;
        pStr++;
    }
}

//******************************************************************************
// I2C Functions ***************************************************************
//******************************************************************************
typedef enum I2C_ModeEnum{
    IDLE_MODE,
    NACK_MODE,
    TX_REG_ADDRESS_MODE,
    RX_REG_ADDRESS_MODE,
    TX_DATA_MODE,
    RX_DATA_MODE,
    SWITCH_TO_RX_MODE,
    SWITHC_TO_TX_MODE,
    TIMEOUT_MODE
} I2C_Mode;

/* Used to track the state of the software state machine*/
I2C_Mode MasterMode = IDLE_MODE;

uint8_t TransmitRegAddr = 0; //Register address for transmission
uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0}; //Buffer for received values
uint8_t RXByteCtr = 0; //Count received bytes
uint8_t ReceiveIndex = 0; //Index of received data
uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0}; //Buffer for transmitted values
uint8_t TXByteCtr = 0; //Count transmitted bytes
uint8_t TransmitIndex = 0; //Index of transmitted data

void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
    uint8_t copyIndex = 0;
    for (copyIndex = 0; copyIndex < count; copyIndex++)
    {
        dest[copyIndex] = source[copyIndex];
    }
}

I2C_Mode I2C_Master_ReadReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t count)
{
    //printf("R\n");
    /* Initialize state machine */
    MasterMode = TX_REG_ADDRESS_MODE;
    TransmitRegAddr = reg_addr;
    RXByteCtr = count;
    TXByteCtr = 0;
    ReceiveIndex = 0;
    TransmitIndex = 0;

    /* Initialize slave address and interrupts */
    UCB1I2CSA = dev_addr;
    UCB1IFG &= ~(UCTXIFG + UCRXIFG);       // Clear any pending interrupts
    UCB1IE &= ~UCRXIE;                       // Disable RX interrupt
    UCB1IE |= UCTXIE;                        // Enable TX interrupt

    UCB1CTLW0 |= UCTR + UCTXSTT;             // I2C TX, start condition
    __bis_SR_register(LPM0_bits + GIE);              // Enter LPM0 w/ interrupts
 //   UCB1IE &= ~UCRXIE;                       // Disable RX interrupt


    return MasterMode;

}

I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
    /* Initialize state machine */
    MasterMode = TX_REG_ADDRESS_MODE;
    TransmitRegAddr = reg_addr;

    //Copy register data to TransmitBuffer
    CopyArray(reg_data, TransmitBuffer, count);

    TXByteCtr = count;
    RXByteCtr = 0;
    ReceiveIndex = 0;
    TransmitIndex = 0;

    /* Initialize slave address and interrupts */
    UCB1I2CSA = dev_addr;
    UCB1IFG &= ~(UCTXIFG + UCRXIFG);       // Clear any pending interrupts
    UCB1IE &= ~UCRXIE;                       // Disable RX interrupt
    UCB1IE |= UCTXIE;                        // Enable TX interrupt

    UCB1CTLW0 |= UCTR + UCTXSTT;             // I2C TX, start condition
    __bis_SR_register(LPM0_bits + GIE);              // Enter LPM0 w/ interrupts
    //printf("W\n");
    return MasterMode;
}

//******************************************************************************
// BMI160 Functions ************************************************************
//******************************************************************************
void bmi160_init(char FOC_axis)
{
    uint8_t writeData[1];
    //Read Chip ID, which is D1
    I2C_Master_ReadReg(SLAVE_ADDR, 0x00, 1);
    if(ReceiveBuffer[0] != 0xD1)
    {
        UART_transmitString(" Incorrect sensor chip ID ");
        printf("Incorrect sensor chip ID\n");
    }




    //Configure the accelerometer
    writeData[0]=0b00101100; //Set acc_us to 0 for off, and acc_bwp must then be 010. Set acc_odr to 1011(800Hz),1100(1600Hz),1000(100Hz),0001(25/32Hz)
    I2C_Master_WriteReg(SLAVE_ADDR, 0x40, writeData, 1);
    //Check if configuration worked
    I2C_Master_ReadReg(SLAVE_ADDR, 0x40, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Accelerometer config failed ");
        printf("Accelerometer config failed\n");
    }
    //Set the range of the accelerometer
    writeData[0]=0b1000; //0b0011 for 2g, 0b0101 for 4g, 0b1000 for 8g
    I2C_Master_WriteReg(SLAVE_ADDR, 0x41, writeData, 1);
    //Check if range is set
    I2C_Master_ReadReg(SLAVE_ADDR, 0x41, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Accelerometer range set failed ");
        printf("Accelerometer range set failed\n");
    }

    //Any motion setup

    //Set the successive slope threshold
    writeData[0]=0b00000001; //0b00000001 + 1 so two successive slopes
    I2C_Master_WriteReg(SLAVE_ADDR, 0x5F, writeData, 1);
    //Check if slope threshold is set
    I2C_Master_ReadReg(SLAVE_ADDR, 0x5F, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Slope threshold not set ");
        printf("Slope threshold not set\n");
    }
    //Set trigger level
    writeData[0]=0b01001101; //15.63mg*value for 8g range, 0b00000000 gives 7.81mg
    I2C_Master_WriteReg(SLAVE_ADDR, 0x60, writeData, 1);
    //Check trigger is set
    I2C_Master_ReadReg(SLAVE_ADDR, 0x60, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Trigger not set ");
        printf("Trigger not set\n");
    }

    //Double tap setup

    //Set single and double tap timings
    writeData[0] = 0b00000110; //Quiet of 30ms, shock of 50ms, double tap within 500ms
    I2C_Master_WriteReg(SLAVE_ADDR, 0x63, writeData, 1);
    //Read the timings
    I2C_Master_ReadReg(SLAVE_ADDR, 0x63, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Tap timings not set ");
        printf("Tap timings not set\n");
    }
    //Set tap threshold
    writeData[0] = 0b0000; //125mg threshold
    I2C_Master_WriteReg(SLAVE_ADDR, 0x64, writeData, 1);
    //Read the threshold
    I2C_Master_ReadReg(SLAVE_ADDR, 0x64, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Tap timings not set ");
        printf("Tap timings not set\n");
    }

    //Interrupt setup

    //Enable any-motion and double tap interrupts
    writeData[0] = 0b00010100; //Enables double tap and any-motion z interrupt
    I2C_Master_WriteReg(SLAVE_ADDR, 0x50, writeData, 1);
    //Read interrupt enable status
    I2C_Master_ReadReg(SLAVE_ADDR, 0x50, 1);
    if(ReceiveBuffer[0] != 0b00010100)
    {
        UART_transmitString("Interrupts not enabled");
        printf("Interrupts not enabled\n");
    }
    //Set pins
    writeData[0] = 0b10001000; //Output, push-pull, active low for int1 and int2
    I2C_Master_WriteReg(SLAVE_ADDR, 0x53, writeData, 1);
    //Read pin status
    I2C_Master_ReadReg(SLAVE_ADDR, 0x53, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Pins not set ");
        printf("Pins not set\n");
    }
    //Set interrupts to temporary instead of latched (permanent till cleared)
    writeData[0] = 0b1101; //Temp for 1.28s
    I2C_Master_WriteReg(SLAVE_ADDR, 0x54, writeData, 1);
    //Check interrupts
    I2C_Master_ReadReg(SLAVE_ADDR, 0x54, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Interrupts not temp ");
        printf("Interrupts not temp");
    }
    //Map any motion detection to Int1
    writeData[0] = 0b00000100; //Mapped any motion to int1
    I2C_Master_WriteReg(SLAVE_ADDR, 0x55, writeData, 1);
    //Check interrupt
    I2C_Master_ReadReg(SLAVE_ADDR, 0x55, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Any motion not mapped ");
        printf("Any motion not mapped\n");
    }
    //Map double tap to Int2
    writeData[0] = 0b00010000; //Mapped double tap to int2
    I2C_Master_WriteReg(SLAVE_ADDR, 0x57, writeData, 1);
    //Check interrupt
    I2C_Master_ReadReg(SLAVE_ADDR, 0x57, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Double tap not mapped ");
        printf("Double tap not mapped\n");
    }
    //Set tap data filtering
    writeData[0] = 0b1000; //Filtered data instead of pre-filtered
    I2C_Master_WriteReg(SLAVE_ADDR, 0x58, writeData, 1);
    //Check filtering
    I2C_Master_ReadReg(SLAVE_ADDR, 0x58, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Filter not set ");
        printf("Filter not set\n");
    }
    //Set the Accelerometer to normal power mode
    writeData[0] = 0x11;
    I2C_Master_WriteReg(SLAVE_ADDR, 0x7E, writeData, 1);
    //Read power mode status of sensors
    I2C_Master_ReadReg(SLAVE_ADDR, 0x03, 1);
    if(ReceiveBuffer[0] != 0x10)
    {
        UART_transmitString(" Accelerometer not on ");
        printf("Accelerometer not on\n");
    }

    //Fast Offset Compensation (FOC) setup

    //0 for reserved, 0 for gyroscope, 00 for x, 00 for y, 0 for z (10 = -1g, 00 = 0g, 01 = 1g)
    switch(FOC_axis)
    {
        case 'X':
            writeData[0] = 0b00100000;
            break;
        case 'Y':
            writeData[0] = 0b00001000;
            break;
        case 'Z':
            writeData[0] = 0b00000010;
            break;
        default:
            writeData[0] = 0b00000000; //Default of all 0g
            break;
    }
    I2C_Master_WriteReg(SLAVE_ADDR, 0x69, writeData, 1);
    //Check FOC
    I2C_Master_ReadReg(SLAVE_ADDR, 0x69, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" FOC not set ");
        printf("Incorrect sensor chip ID\n");
    }
    //Start FOC
    writeData[0] = 0x03;
    I2C_Master_WriteReg(SLAVE_ADDR, 0x7E, writeData, 1);
    //Wait until FOC is finished
    int finish = 0;
    while(finish==0)
    {
        I2C_Master_ReadReg(SLAVE_ADDR, 0x1B, 1);
        if((ReceiveBuffer[0] & 0b00001000) == 0b00001000)
        {
            finish = 1;
        }
    }
    //Enable offset compensation
    writeData[0] = 0b01000000; //Enable accelerometer offset compensation
    I2C_Master_WriteReg(SLAVE_ADDR, 0x77, writeData, 1);
    //Check offset compensation
    I2C_Master_ReadReg(SLAVE_ADDR, 0x77, 1);
    if(ReceiveBuffer[0] != writeData[0])
    {
        UART_transmitString(" Offset not enabled ");
        printf("Incorrect sensor chip ID\n");
    }
    //UART_transmitString(" BMI160 Initialized \n");
}



//******************************************************************************
// Device Initialization *******************************************************
//******************************************************************************
void initGPIO()
{
    /* Terminate all GPIO pins to Output LOW to minimize power consumption */
    GPIO_setAsOutputPin(GPIO_PORT_PA, GPIO_PIN_ALL16);
    GPIO_setAsOutputPin(GPIO_PORT_PB, GPIO_PIN_ALL16);
    GPIO_setAsOutputPin(GPIO_PORT_PC, GPIO_PIN_ALL16);
    GPIO_setAsOutputPin(GPIO_PORT_PD, GPIO_PIN_ALL16);
    GPIO_setAsOutputPin(GPIO_PORT_PE, GPIO_PIN_ALL16);
    GPIO_setAsOutputPin(GPIO_PORT_PF, GPIO_PIN_ALL16);
    GPIO_setOutputLowOnPin(GPIO_PORT_PA, GPIO_PIN_ALL16);
    GPIO_setOutputLowOnPin(GPIO_PORT_PB, GPIO_PIN_ALL16);
    GPIO_setOutputLowOnPin(GPIO_PORT_PC, GPIO_PIN_ALL16);
    GPIO_setOutputLowOnPin(GPIO_PORT_PD, GPIO_PIN_ALL16);
    GPIO_setOutputLowOnPin(GPIO_PORT_PE, GPIO_PIN_ALL16);
    GPIO_setOutputLowOnPin(GPIO_PORT_PF, GPIO_PIN_ALL16);

    // I2C pins (P4.0 is SDA, P4.1 is SCL)
    P4SEL1 |= BIT0 | BIT1;
    P4SEL0 &= ~(BIT0 | BIT1);

    // Configure P3.4 and P3.5 to UART (Primary, TX and RX respectively) for NeoCortec
    P3SEL0 |= BIT4 | BIT5;                    // USCI_A1 UART operation
    P3SEL1 &= ~(BIT4 | BIT5);                 // SEL1 is 0 and SEL0 is 1 for primary operation, inverse for secondary

    // Configure P2.0 and P2.1 to UART (Primary, TX and RX respectively) for PC
    P2SEL0 |= BIT0 | BIT1;                    // USCI_A0 UART operation
    P2SEL1 &= ~(BIT0 | BIT1);                 // SEL1 is 0 and SEL0 is 1 for primary operation, inverse for secondary

    // Configure button S1 (P1.1) interrupt
    GPIO_selectInterruptEdge(GPIO_PORT_P1, GPIO_PIN1, GPIO_HIGH_TO_LOW_TRANSITION);
    GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN1);
    GPIO_clearInterrupt(GPIO_PORT_P1, GPIO_PIN1);
    GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN1);

    // Configure button S2 (P1.2) interrupt
    GPIO_selectInterruptEdge(GPIO_PORT_P1, GPIO_PIN2, GPIO_HIGH_TO_LOW_TRANSITION);
    GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN2);
    GPIO_clearInterrupt(GPIO_PORT_P1, GPIO_PIN2);
    GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN2);

    // Configure CTS active (P1.3) interrupt
    GPIO_selectInterruptEdge(GPIO_PORT_P1, GPIO_PIN3, GPIO_HIGH_TO_LOW_TRANSITION);
    GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN3);
    GPIO_clearInterrupt(GPIO_PORT_P1, GPIO_PIN3);
    GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN3);

    // Configure Nwu (P1.4) interrupt
    GPIO_selectInterruptEdge(GPIO_PORT_P1, GPIO_PIN4, GPIO_HIGH_TO_LOW_TRANSITION);
    GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN4);
    GPIO_clearInterrupt(GPIO_PORT_P1, GPIO_PIN4);
    GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN4);

    // Configure INT1 (P3.2) interrupt
    GPIO_selectInterruptEdge(GPIO_PORT_P3, GPIO_PIN2, GPIO_HIGH_TO_LOW_TRANSITION);
    GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P3, GPIO_PIN2);
    GPIO_clearInterrupt(GPIO_PORT_P3, GPIO_PIN2);
    GPIO_enableInterrupt(GPIO_PORT_P3, GPIO_PIN2);

    // Configure INT2 (P2.5) interrupt
    GPIO_selectInterruptEdge(GPIO_PORT_P2, GPIO_PIN5, GPIO_HIGH_TO_LOW_TRANSITION);
    GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P2, GPIO_PIN5);
    GPIO_clearInterrupt(GPIO_PORT_P2, GPIO_PIN5);
    GPIO_enableInterrupt(GPIO_PORT_P2, GPIO_PIN5);

    // Disable the GPIO power-on default high-impedance mode to activate
    // previously configured port settings
    PM5CTL0 &= ~LOCKLPM5;
    __bis_SR_register(GIE);
}

void initClockTo16MHz()
{
    // Configure one FRAM waitstate as required by the device datasheet for MCLK
    // operation beyond 8MHz _before_ configuring the clock system.
    FRCTL0 = FRCTLPW | NWAITS_1;

    // Clock System Setup
    CSCTL0_H = CSKEY_H;                     // Unlock CS registers
    CSCTL1 = DCOFSEL_0;                     // Set DCO to 1MHz

    // Set SMCLK = MCLK = DCO, ACLK = VLOCLK (9.4kHz)
    CSCTL2 = SELA__VLOCLK | SELS__DCOCLK | SELM__DCOCLK;

    // Per Device Errata set divider to 4 before changing frequency to
    // prevent out of spec operation from overshoot transient
    CSCTL3 = DIVA__4 | DIVS__4 | DIVM__4;   // Set all corresponding clk sources to divide by 4 for errata
    CSCTL1 = DCOFSEL_4 | DCORSEL;           // Set DCO to 16MHz

    // Delay by ~10us to let DCO settle. 60 cycles = 20 cycles buffer + (10us / (1/4MHz))
    __delay_cycles(60);
    CSCTL3 = DIVA__32 | DIVS__1 | DIVM__1;  // Set ACLK to 239.75Hz, SMCLK to 16MHz, and MCLK to 16MHz
    CSCTL0_H = 0;                           // Lock CS registers
}

void initI2C()
{
    UCB1CTLW0 = UCSWRST;                      // Enable SW reset
    UCB1CTLW0 |= UCMODE_3 | UCMST | UCSSEL__SMCLK | UCSYNC; // I2C master mode, SMCLK
    UCB1BRW = 160;                            // fSCL = ACLK/160 = ~100kHz
    UCB1I2CSA = SLAVE_ADDR;                   // Slave Address
    UCB1CTLW0 &= ~UCSWRST;                    // Clear SW reset, resume operation
    UCB1IE |= UCNACKIE;
}

void UART_init(void)
{
    // Configure USCI_A1 for UART mode
    UCA1CTLW0 = UCSWRST;                      // Put eUSCI in reset
    UCA1CTLW0 |= UCSSEL__SMCLK;               // CLK = SMCLK
    UCA1BR0 = 8;                              // Clock prescaler set to 8
    UCA1BR1 = 0x00;                           // High byte empty, low byte is 8
    UCA1MCTLW |= UCOS16 | UCBRF_10 | 0xF700;  // Over-sampling on, first modulation register set to 10, second modulation register set to 0xF7 (247) for high byte, 0 for low byte
    UCA1CTLW0 &= ~UCSWRST;                    // Initialize eUSCI
    UCA1IE |= UCRXIE;                         // Enable USCI_A1 RX interrupt

    // Configure USCI_A0 for UART mode
    UCA0CTLW0 = UCSWRST;                      // Put eUSCI in reset
    UCA0CTLW0 |= UCSSEL__SMCLK;               // CLK = SMCLK
    UCA0BR0 = 8;                              // Clock prescaler set to 8
    UCA0BR1 = 0x00;                           // High byte empty, low byte is 8
    UCA0MCTLW |= UCOS16 | UCBRF_10 | 0xF700;  // Over-sampling on, first modulation register set to 10, second modulation register set to 0xF7 (247) for high byte, 0 for low byte
    UCA0CTLW0 &= ~UCSWRST;                    // Initialize eUSCI
    UCA0IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
}



//******************************************************************************
// Main ************************************************************************
//******************************************************************************

 int main(void)
 {
    WDTCTL = WDTPW | WDTHOLD;   // Stop watchdog timer
    //Initialize all peripherals
    initClockTo16MHz();
    initGPIO();
    UART_init();
    initI2C();

    bmi160_init('Z');

    // Initialize the FFT parameters
    msp_status status;
    msp_fft_q15_params fftParams;

    /* Initialize the fft parameter structure. */
    fftParams.length = SAMPLES;
    fftParams.bitReverse = true;
    fftParams.twiddleTable = msp_cmplx_twiddle_table_4096_q15; //Twiddle table for 4096 values


    int i = 0;

    //new
    TA0CTL   = TA0CTL | (SMCLK + CONTINUOUS);           // SMCLK:  Counts faster than ACLK
                                                        // CONTINUOUS:  Count 0 to 0xFFFF
    TA0CCTL0 = CCIE;                                    // Timer_0 interrupt

    TA1CTL   = TA1CTL | (ACLK  + UP         );          // Count up from 0 with ACLK
    TA1CCR0  = MS_10;                                   // Duration approximatley 10ms

    _BIS_SR(GIE);                                       // Activate all interrupts

    //new

    while(1)
    {
           printf("Reading samples\n");
           //Read SAMPLES amount of data from the BMI160
           for(i=0;i<SAMPLES;i++)
           {
               I2C_Master_ReadReg(SLAVE_ADDR, 0x16, 2); //Read the acceleration value from the BMI160 registers
               input[i]= ReceiveBuffer[0] | (ReceiveBuffer[1] << 8); //Store the value in an array
               //delay_ms(1); //Determines sampling frequency, up to 10kHz
               __delay_cycles(4500);
               //printf("Sent acc: %u\n",input[i]);
           }
           printf("Samples read\n");


           msp_benchmarkStart(MSP_BENCHMARK_BASE, 16);
           status = msp_fft_fixed_q15(&fftParams, input); //Perform FFT
           cycleCount = msp_benchmarkStop(MSP_BENCHMARK_BASE);
           msp_checkStatus(status);
           printf("FFT completed\n");

           //Transmit all output values to PC


       //Calculate and transmit frequencies with maximum amplitudes
       getMaximums(input, SAMPLES, max, amp);
       printf("Max amp frequencies found\n");


       // Transmit top 5 frequencies via NeoCortec
       for(i=0; i<5; i++)
       {
           printf("Sent freq: %u\n", (unsigned int)max[i]);
       }


       GPIO_toggleOutputOnPin(GPIO_PORT_P1, GPIO_PIN0);
       // Transmit matching amplitudes
       for(i=0; i<5; i++)
       {
           printf("Sent amp: %u\n", (unsigned int)amp[i]);
       }
    }
}


//******************************************************************************
// Interrupts ******************************************************************
//******************************************************************************

//I2C Interrupt
#pragma vector = USCI_B1_VECTOR
__interrupt void USCI_B1_ISR(void)
{
  //Must read from UCB1RXBUF
  uint8_t rx_val = 0;
  switch(__even_in_range(UCB1IV, USCI_I2C_UCBIT9IFG))
  {
    case USCI_NONE:          break;         // Vector 0: No interrupts
    case USCI_I2C_UCALIFG:   break;         // Vector 2: ALIFG
    case USCI_I2C_UCNACKIFG:                // Vector 4: NACKIFG
      UCB1CTLW0 |= UCTXSTT;                 // Re-send start if NACK
      break;
    case USCI_I2C_UCSTTIFG:  break;         // Vector 6: STTIFG
    case USCI_I2C_UCSTPIFG:  break;         // Vector 8: STPIFG
    case USCI_I2C_UCRXIFG3:  break;         // Vector 10: RXIFG3
    case USCI_I2C_UCTXIFG3:  break;         // Vector 12: TXIFG3
    case USCI_I2C_UCRXIFG2:  break;         // Vector 14: RXIFG2
    case USCI_I2C_UCTXIFG2:  break;         // Vector 16: TXIFG2
    case USCI_I2C_UCRXIFG1:  break;         // Vector 18: RXIFG1
    case USCI_I2C_UCTXIFG1:  break;         // Vector 20: TXIFG1
    case USCI_I2C_UCRXIFG0:                 // Vector 22: RXIFG0
        rx_val = UCB1RXBUF;
        if (RXByteCtr)
        {
          ReceiveBuffer[ReceiveIndex++] = rx_val;
          RXByteCtr--;
        }

        if (RXByteCtr == 1)
        {
          UCB1CTLW0 |= UCTXSTP;
        }
        else if (RXByteCtr == 0)
        {
          UCB1IE &= ~UCRXIE;
          MasterMode = IDLE_MODE;
          __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
        }
        break;
    case USCI_I2C_UCTXIFG0:                 // Vector 24: TXIFG0
        switch (MasterMode)
        {
          case TX_REG_ADDRESS_MODE:
              UCB1TXBUF = TransmitRegAddr;
              if (RXByteCtr)
                  MasterMode = SWITCH_TO_RX_MODE;   // Need to start receiving now
              else
                  MasterMode = TX_DATA_MODE;        // Continue to transmision with the data in Transmit Buffer
              break;

          case SWITCH_TO_RX_MODE:
              UCB1IE |= UCRXIE;              // Enable RX interrupt
              UCB1IE &= ~UCTXIE;             // Disable TX interrupt
              UCB1CTLW0 &= ~UCTR;            // Switch to receiver
              MasterMode = RX_DATA_MODE;    // State state is to receive data
              UCB1CTLW0 |= UCTXSTT;          // Send repeated start
              if (RXByteCtr == 1)
              {
                  //Must send stop since this is the N-1 byte
                  while((UCB1CTLW0 & UCTXSTT));
                  UCB1CTLW0 |= UCTXSTP;      // Send stop condition
              }
              break;

          case TX_DATA_MODE:
              if (TXByteCtr)
              {
                  UCB1TXBUF = TransmitBuffer[TransmitIndex++];
                  TXByteCtr--;
              }
              else
              {
                  //Done with transmission
                  UCB1CTLW0 |= UCTXSTP;     // Send stop condition
                  MasterMode = IDLE_MODE;
                  UCB1IE &= ~UCTXIE;                       // disable TX interrupt
                  __bic_SR_register_on_exit(CPUOFF);      // Exit LPM0
              }
              break;

          default:
              __no_operation();
              break;
        }
        break;
    default: break;
  }
}


#pragma vector = PORT2_VECTOR
__interrupt void PORT2_ISR(void)
{
    switch(__even_in_range(P2IV, P2IV_P2IFG7))
       {
           case P2IV_NONE : break;
           case P2IV_P2IFG0 : break;
           case P2IV_P2IFG1 : break;
           case P2IV_P2IFG2 : break;
           case P2IV_P2IFG3 : break;
           case P2IV_P2IFG4 : break;
           case P2IV_P2IFG5 :       //Int2 sensor interrupt
               P2IFG = P2IFG & ~(BIT2);
               break;
           case P2IV_P2IFG6 : break;
           case P2IV_P2IFG7 : break;
           default : _never_executed();
       }
}


// Timer_0 Interrupt Service Routine
#pragma vector=TIMER0_A0_VECTOR
__interrupt void Timer_A0 (void)
{
    TA0CTL = TA0CTL & (~TAIFG);       // Reset Timer_0 so it keeps counting
}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好

    // FFT 样本数
    define samples 4096

    如果由于2KB RAM 限制将样本更改为512个样本、您能否 hlep 测试它是否正常工作

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的建议、Xiaodong LI。 更改该值后、有时我会得到接近3.5Hz 的值、有时我会得到随机值。 这就是为什么我不确定它是否正常工作的原因。 此外、当我将频率增加到4、6或9Hz 时、它会再次返回显示随机值。 因此、更改采样编号可能没有帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好

    如果只是减少不起作用的样本数量、我需要几天时间来查看代码。 我稍后会回答您的问题。

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常感谢;非常感谢您的帮助。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    此外、我 不确定、但由于我 要将数据存储在 FRAM 中、因此样本数量可能不是问题所在。  

      

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好

    感谢您提供的信息、我将查看代码并检查这一点。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢你

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好

    我已查看您的存储器分配屏幕截图、

    请问您在这里采用了什么样片编号? 它是4K 字节还是1K 字节?

    我不知道为什么 FRAM2的大小为~26KB。

    如果不确定数据是否存储在 FRAM 中、可以尝试通过 CCS 上的 View -> Memory Brower 检查数据。

    我检查了您的代码、但我没有从代码中找到线索

    以下是 DSPLib 和 FFT 的用户指南供参考: https://dev.ti.com/tirex/explore/node?node=APFYDDVAZQjSJ7vLKa8XPg__IOGqZri__LATEST

    谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    谢谢你。 我要获取4096 个样本。  

    [引用 userid="125557" URL"~/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1128408/msp430fr6989-fft-analysis-using-dsplib-h/4199472 #4199472"]我不知道为什么 FRAM2大小是~26KB。

    我不知道你的意思是什么。 如果您能更详细地解释数据、我将不胜感激。 此 MCU 的总 FRAM 为128KB。

    不过、我有一个问题、是否有直接方法将采样频率传递到 FFT 计算?

    [引用 userid="125557" URL"~/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1128408/msp430fr6989-fft-analysis-using-dsplib-h/4199472 #4199472"]以下是 DSPLIB 和 FFT 的用户指南供参考:

    我已经看到过它、但仍然找不到问题。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    您是否在 DSPLIB 中尝试过 FFT 示例?

    对于 FFT、信号频率、采样频率和长度存在一些释放性、否则会遇到一些问题。  

    我想您可以检查示例代码是否正常。

    谢谢!

    此致

    Johnson

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的回复。 我看到了这个示例。 问题是、我已经阅读了许多 FFT 分析理论。 但是、当我尝试将它们与 C 编程语言示例进行比较时、我无法与它们相关。 示例代码没有解释或试图将概念与代码关联起来、我希望您已经了解我要解释的内容。 现在、我感觉从一开始就开始了。 因此、请记住参考示例:

    我将在数组中保存4096个样本。 我还可以从 BMI160获取加速计数据的确切时间戳。 因此、如果我获取两个相应样本之间的差异或在总时间内求平均值、我将获得采样率。 如果我错了、请纠正我的问题。

    从这一点开始、我有点迷路了。 起初、我以为我需要将采样频率和样本传递到"MSP_FFT_FIXED_Q15 ()"函数、这样就完成了该过程。 但"MSP_FFT_FIXED_Q15 ()"似乎仅接受样本作为输入、而不是采样频率。 这就是为什么我不确定"MSP_FFT_FIXED_Q15 ()"函数的输出结果是什么、以及如何稍后使用采样频率来找到最终的 FFT 值。  

    让我们假设我以16.029ms 的间隔获取每个样本。

    因此、我的采样频率为1/0.016029s = 62.3869237Hz。

    由于采样率为62.3869237 Hz、带宽将为62.3869237/2 = 31.1935Hz (不确定)。

    当我采集4096个样本时、箱数将为4096/2 = 2048。

    因此、容器大小将为31.1935/2048 = 0.0152 (不确定)。

    这是我根据自己的理解进行的计算。 如果有人告诉我计算是否正确、我将不胜感激。

    现在、我不确定如何使用这些值来使用"MSP_FFT_FIXED_Q15 ()"函数执行 FFT。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    "由于采样率为62.3869237Hz、带宽将为62.3869237/2 = 31.1935Hz (不确定)。"

    *您*控制带宽。 如果您希望采样频率为62Hz、则必须对信号进行滤波、以便没有高于31Hz 的信号、否则会出现混叠。 例如、我熟悉的 TM 具有截止频率为4000Hz 的加速器通道滤波器和17000Hz 的采样率。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    感谢您的善意回应。 有一个选项可以为传感器选择带宽和滤波-3dB 点、我已经相应地选择了它们。 但我的问题是如何将前面提到的变量(采样频率、带宽、箱数、箱大小)与"MSP_FFT_FIXED_Q15()"函数结合使用? 我不确定"MSP_FFT_FIXED_Q15 ()"函数是如何工作的、将数据传递给函数后需要什么样的输出以及后续的操作。 如果您能解释如何执行 FFT 操作、然后使用这些变量和"MSP_FFT_FIXED_Q15()"函数获取 FFT 值、我将不胜感激。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    根据您的建议、我对代码进行了一些修改、现在我获得了很好的结果。 我的测试平台以大约3.3~3.5 Hz 的频率振动。 当我采集512个样本和1024个样本时、我会得到很好的结果。

    512个样本:最大 FFT 3Hz

    1024个样本:3Hz 时的最大 FFT

    但对于4096个样本、我会得到错误的读取。

    4096个样本:17 Hz 时的 MAZ FFT

    BMI160有一个内部计数器、该计数器以39us 的间隔递增计数器。 因此、我使用它作为每个数据点的时间戳、采样频率为933.42Hz。  

     

    根据 BMI160数据表、我意识到可能需要使用几个变量来执行精确计算。 一个是带宽(第19页)、第二个是加速计范围(第59页)。

     

    带宽:由于采样频率为933.42Hz、因此我的带宽应为466.71Hz。 因此、我选择了1600 ODR 值(Z 轴)。

      

    加速计范围:不确定选择哪一个以及原因。

    尽管我逐渐了解该流程的工作原理、但我仍有几个问题:

    1、4096采样程序为何偏离实际值? (我认为使用较高的样本时、我应该得到更宝贵的值)

    2、如何计算 FFT (小数点)更珍贵的值?

    3.我可以使用浮点值执行 FFT 吗? (由于实际 FFT 值应为3.3Hz~ 3.5Hz)

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    假设每个区间为 Hz、实际上是 FS/numsamples、则您的假设是错误的。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Keith、您好、在短暂休息后回到了项目。 感谢您的回复。 您可能会对您的评论再详细阐述一下吗? 我想、在执行 FFT 之后、我实际上会接收到实际的频率值。 您是否说我实际收到了 bin 编号?

    还有、我可以 使用浮点值执行 FFT 吗? (实际振动频率为3.3Hz~ 3.5Hz)。 基于此链接:

    https://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430Ware/3_50_00_04/exports/MSP430Ware_3_50_00_04/MSP430Ware_win/dsplib/html/usage.html

    看起来我应该能够得到小数值。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Ahammand、

    此问题是否已解决?  

    谢谢!

    此致

    Johnson