请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:MSP430FR6043 大家好、
以下是客户提出的问题、可能需要您的帮助:
位置:\ti\MSP\USS_02_40_00_00\USS\examples\USSSWLib_template_examples\ccs
项目: FR6043_USSSWLib_TEMPLE_example
文件: ussSwLib.h
//! \brief This defines the capture sequence selection CH0 #define USS_CAPTURE_SEQUENCE_SELECTION_CH0 0 //! \brief This defines the capture sequence selection CH1 #define USS_CAPTURE_SEQUENCE_SELECTION_CH1 1 //! \brief This defines the capture sequence selection CH0_CH1 #define USS_CAPTURE_SEQUENCE_SELECTION_CH0_CH1 2 //! \brief This defines the capture sequence selection CH1_CH0 #define USS_CAPTURE_SEQUENCE_SELECTION_CH1_CH0 3 //! \brief This defines the capture sequence selection CH0_CH0 #define USS_CAPTURE_SEQUENCE_SELECTION_CH0_CH0 4 //! \brief This defines the capture sequence selection CH1_CH1 #define USS_CAPTURE_SEQUENCE_SELECTION_CH1_CH1 5 //! \brief This defines the capture sequence selection CH0_CH1_CH0 #define USS_CAPTURE_SEQUENCE_SELECTION_CH0_CH1_CH0 6 //! \brief This defines the capture sequence selection CH1_CH0_CH1 #define USS_CAPTURE_SEQUENCE_SELECTION_CH1_CH0_CH1 7 //! \brief This defines the capture sequence selection CH0_CH0_CH0 #define USS_CAPTURE_SEQUENCE_SELECTION_CH0_CH0_CH0 8 //! \brief This defines the capture sequence selection CH1_CH1_CH1 #define USS_CAPTURE_SEQUENCE_SELECTION_CH1_CH1_CH1 9 //! \brief This defines the capture sequence selection CH0_CH1_CH0_CH1 #define USS_CAPTURE_SEQUENCE_SELECTION_CH0_CH1_CH0_CH1 10 //! \brief This defines the capture sequence selection CH1_CH0_CH1_CH0 #define USS_CAPTURE_SEQUENCE_SELECTION_CH1_CH0_CH1_CH0 11 //! \brief This defines the capture sequence selection CH0_CH0_CH0_CH0 #define USS_CAPTURE_SEQUENCE_SELECTION_CH0_CH0_CH0_CH0 12 //! \brief This defines the capture sequence selection CH1_CH1_CH1_CH1 #define USS_CAPTURE_SEQUENCE_SELECTION_CH1_CH1_CH1_CH1 13
这些 不同定义对应的信号序列是什么?
谢谢、此致
耶鲁李