请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:MSP432E401Y 大家好、我需要将2个 MSP432E401Y 连接到一个以太网端口、我想只需在 MCU#2上的变压器介质侧与 MCU#1介质侧之间运行布线即可。我知道我可以使用开关、但在我考虑之前需要寻找其他选项。感谢您的任何输入
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、我需要将2个 MSP432E401Y 连接到一个以太网端口、我想只需在 MCU#2上的变压器介质侧与 MCU#1介质侧之间运行布线即可。我知道我可以使用开关、但在我考虑之前需要寻找其他选项。感谢您的任何输入