本产品的新特性(MSP-EXP430G2 LaunchPad 开发套件修订版1.5)。
能否卸下电路板底部的10引脚母连接器(断开或断开焊料?)。 需要将电路板平放在4个橡胶角上。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本产品的新特性(MSP-EXP430G2 LaunchPad 开发套件修订版1.5)。
能否卸下电路板底部的10引脚母连接器(断开或断开焊料?)。 需要将电路板平放在4个橡胶角上。
Wei、
感谢你的答复。 您提到我可以移除连接器...
我是否可以仅卸下底部的"母连接器",或者是否必须卸下整个公连接器/母连接器?
如果我必须卸下整个公接头/母接头..... 我能否单独“或”解焊每一个,我是否必须同时解焊全部10个...我不知道我是否可以这样做?
如果你说我一次只能做一个,那么底部的插头会... 是否与相邻的公连接器断开?
我需要做的是、顶部有6个公连接器、底部没有任何母连接器。
在下面的网站中,如果您可以向下滚动到名为“步骤3:将大气压力传感器分线板焊接到 MSP430 Launchpad”的段落,下面的第一张照片中的步骤3就是我要做的事情。
网址: www.uswaterrockets.com/.../manual.htm
请原谅我这些非常基本的问题 我是电路板的"新手"。
感谢你的帮助。
Richard