请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:MSP430FR2433 我刚刚~了 P1DIR &=Δ I BIT0、并观察到、即使我有一个4K 上拉至3.3、信号也是1.8V
当我更改为 P1DIR |= BIT0时、信号下降至0V
我还应该做些什么来使输入引脚保持高电平?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我刚刚~了 P1DIR &=Δ I BIT0、并观察到、即使我有一个4K 上拉至3.3、信号也是1.8V
当我更改为 P1DIR |= BIT0时、信号下降至0V
我还应该做些什么来使输入引脚保持高电平?