请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TRF7970A 您好、专家、
我还有一个来自客户的问题,关于可选输出功率级别,我们只有两个选项:+20dBm 或+23dBm ?
数据表显示。 '当使用5V 电源时、发送器具有等效于50 Ω 负载的100mW (+20dBm)或200mW (+23dBm)的可选输出功率水平。'
问题是,例如,如何设置0dBm 或+10dBm……
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、专家、
我还有一个来自客户的问题,关于可选输出功率级别,我们只有两个选项:+20dBm 或+23dBm ?
数据表显示。 '当使用5V 电源时、发送器具有等效于50 Ω 负载的100mW (+20dBm)或200mW (+23dBm)的可选输出功率水平。'
问题是,例如,如何设置0dBm 或+10dBm……