请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:RF430FRL152H 工具/软件:Code Composer Studio
你好!
当我通过移除 RFPMMCTL0中的 EN_V_dob 来禁用 VDD2X 时、VDD2X 的电势仍为1.3V。 是否可以将其配置为0V?
谢谢、
Nico
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:Code Composer Studio
你好!
当我通过移除 RFPMMCTL0中的 EN_V_dob 来禁用 VDD2X 时、VDD2X 的电势仍为1.3V。 是否可以将其配置为0V?
谢谢、
Nico