Other Parts Discussed in Thread: TPS62932
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS62932 工具/软件:
尊敬的团队:
您能帮助检查 TPS62932是否能够满足以下要求吗? 谢谢。
VIN=12V-18V
Vout=-9V
600mA = Iout/IOUT/ 300mA
效率>80%
BR。
Frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.