This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ40Z80:BQ40z80显示了与电池组不同的电压和电流

Guru**** 2815505 points

Other Parts Discussed in Thread: BQ40Z80, BQSTUDIO, GPCCHEM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1505367/bq40z80-bq40z80-showed-different-voltage-and-current-than-the-pack

产品型号:BQ40Z80
主题中讨论的其他器件: BQSTUDIOGPCCHEM

工具/软件:

我已经使用 BQ40z80制作了一个电池组、并对其进行了编程和设置。 然后断开与电池的连接、由于未知原因、几天后电压显示为65.35V、大约8A 电流放电、实际值是或6节串联电池的23V 电压、70mA 放电稍后才知道它进入密封模式。

有什么原因导致了这种情况?
谢谢