Other Parts Discussed in Thread: BQ40Z80EVM-020, EV2400, BQSTUDIO
主题中讨论的其他器件: EV2400、 BQSTUDIO
工具/软件:
我正在尝试使用 BQ40Z80EVM-020、且连接困难。 到目前为止、我有:
- 将板载 EV2400固件更新为0.32版
- 已尝试外部 EV2400、已成功更新至固件版本0.32
- 尝试在断开电池连接并将3节串联电池连接到 J12的情况下进行连接
- 尝试连接 Battery Management Studio
- 选择4800_0_02-bq40z80.bqz 芯片
- 我收到警告:"检测到的设备与此应用程序不兼容!..."
- 尝试扫描设备或从设备获取信息导致 Battery Management Studio 应用程序崩溃或收到消息"No recognition from device"。
- 以下是来自 SMBD1和 SMBC1跳线的一些通信信号(从外部跳线到内部 EV2400)


- 选择4800_0_02-bq40z80.bqz 芯片
- 试用 Python API 示例并获取以下日志:
PS C:\Program Files (x86)\Texas Instruments\BQ-BATTERY-PROGRAMMER-SW\BQ-BMS-PROGRAMMER-SW\Python_API> & 'C:\Users\COSMED USER\AppData\Local\Programs\Python\Python313-32\python.exe' .\PythonAPIExample.py 2147483647 32 Testing Connect Connecting... Failed to open connection. Windows error code 0x5 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x5 Failed to open connection. Windows error code 0x5 Failed to open connection. Windows error code 0x5 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x5 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x20 Failed to open connection. Windows error code 0x5 Error: Adapter not found!. Error code = 302 Connect result: Connected = False Testing SMBusCommand Failed to open connection. Windows error code 0x3 Failed to reconnect to . Error code = 311 SMBusCommand result: 61 Error 61 Description: 61 ERROR_HANDLE_NOT_INIT // The adapter USB connected was not initialized Testing SMBusWriteWord Failed to open connection. Windows error code 0x3 Failed to reconnect to . Error code = 311 SMBusWriteWord result: 61 Testing SMBusReadWord Failed to open connection. Windows error code 0x3 Failed to reconnect to . Error code = 311 SMBusReadWord result: Failed communication with error code 61 Error 61 Description: 61 ERROR_HANDLE_NOT_INIT // The adapter USB connected was not initialized Testing SMBusWriteBlock Failed to open connection. Windows error code 0x3 Failed to reconnect to . Error code = 311 SMBusWriteBlock result: 61 Testing WaitMilliseconds Testing SMBusReadBlock Failed to open connection. Windows error code 0x3 Failed to reconnect to . Error code = 311 SMBusReadBlock result: Failed communication with error code 61 done PS C:\Program Files (x86)\Texas Instruments\BQ-BATTERY-PROGRAMMER-SW\BQ-BMS-PROGRAMMER-SW\Python_API> & 'C:\Users\COSMED USER\AppData\Local\Programs\Python\Python313-32\python.exe' .\PythonAPIExample.py
系统:
- Windows 11专业版
- Battery Management Studio 版本: 1.3.101.1
问题:
-是否有 bq40z80EVM-020的原理图或设计文件? 我尝试监控从 EV2400进入芯片的信号、并确保监控正确的信号。
-我还应该测试什么?