This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM65645-Q1:电感器选型

Guru**** 2814455 points

Other Parts Discussed in Thread: LM65645

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1514595/lm65645-q1-inductor-selection

器件型号:LM65645-Q1
Thread 中讨论的其他器件:LM65645

工具/软件:

在 TI 的工作台中、如果您设计使用12V 至48V IN 的 LM65645电源和3A 的输出电流、以及3.3V、5V 或12V 作为输出电压、则所有这些电源都使用10uF 电感器。 这与数据表第25页不一致。 应该使用工作台设计还是数据表?

谢谢