请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS1685 工具/软件:
您好、
数据表建议引脚13和19使用33k 上拉电阻。 我的客户希望上拉至3.3V
您知道它是否必须完全为33k、或者使用20k 或10k 等值是否可以?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:
您好、
数据表建议引脚13和19使用33k 上拉电阻。 我的客户希望上拉至3.3V
您知道它是否必须完全为33k、或者使用20k 或10k 等值是否可以?