请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS65219 主题中讨论的其他器件: SK-AM62B-P1
工具/软件:
尊敬的 TI:
我们将 tps65219与 AM62X 一起使用、并使 Kasan 调试不相关的问题、但我注意到弹出了该错误。
Linux 内核在 ti-linux-kernel 中的6.12.22标记为11.00.12。
谢谢、
布莱斯
[ 1.620418] ================================================================== [ 1.620475] BUG: KASAN: slab-out-of-bounds in tps65219_regulator_probe+0x750/0x950 [ 1.620528] Write of size 8 at addr ffff000001f526c8 by task kworker/u4:2/46 [ 1.620547] [ 1.620566] CPU: 0 UID: 0 PID: 46 Comm: kworker/u4:2 Not tainted 6.12.22 #1 [ 1.620591] Hardware name: LandisGyr e370 AM62X (DT) [ 1.620608] Workqueue: async async_run_entry_fn [ 1.620660] Call trace: [ 1.620669] dump_backtrace+0x98/0x118 [ 1.620700] show_stack+0x18/0x24 [ 1.620723] dump_stack_lvl+0x78/0x90 [ 1.620748] print_report+0x118/0x57c [ 1.620776] kasan_report+0xb8/0xfc [ 1.620798] __asan_report_store8_noabort+0x20/0x2c [ 1.620824] tps65219_regulator_probe+0x750/0x950 [ 1.620844] platform_probe+0xc4/0x180 [ 1.620876] really_probe+0x180/0x7d8 [ 1.620898] __driver_probe_device+0x15c/0x364 [ 1.620919] driver_probe_device+0x5c/0x16c [ 1.620941] __device_attach_driver+0x16c/0x270 [ 1.620962] bus_for_each_drv+0x108/0x194 [ 1.620982] __device_attach_async_helper+0x18c/0x230 [ 1.621004] async_run_entry_fn+0x90/0x3ac [ 1.621029] process_one_work+0x524/0xbdc [ 1.621053] worker_thread+0x5f8/0xfbc [ 1.621073] kthread+0x2b8/0x33c [ 1.621091] ret_from_fork+0x10/0x20 [ 1.621113] [ 1.621121] Allocated by task 46 on cpu 0 at 1.619923s: [ 1.621138] kasan_save_stack+0x3c/0x64 [ 1.621162] kasan_save_track+0x24/0x5c [ 1.621182] kasan_save_alloc_info+0x40/0x54 [ 1.621206] __kasan_kmalloc+0xd4/0xd8 [ 1.621225] __kmalloc_node_track_caller_noprof+0x170/0x320 [ 1.621248] devm_kmalloc+0x4c/0x18c [ 1.621267] tps65219_regulator_probe+0x3c4/0x950 [ 1.621286] platform_probe+0xc4/0x180 [ 1.621309] really_probe+0x180/0x7d8 [ 1.621328] __driver_probe_device+0x15c/0x364 [ 1.621348] driver_probe_device+0x5c/0x16c [ 1.621369] __device_attach_driver+0x16c/0x270 [ 1.621389] bus_for_each_drv+0x108/0x194 [ 1.621408] __device_attach_async_helper+0x18c/0x230 [ 1.621429] async_run_entry_fn+0x90/0x3ac [ 1.621453] process_one_work+0x524/0xbdc [ 1.621472] worker_thread+0x5f8/0xfbc [ 1.621492] kthread+0x2b8/0x33c [ 1.621508] ret_from_fork+0x10/0x20 [ 1.621526] [ 1.621534] The buggy address belongs to the object at ffff000001f52600 [ 1.621534] which belongs to the cache kmalloc-192 of size 192 [ 1.621551] The buggy address is located 8 bytes to the right of [ 1.621551] allocated 192-byte region [ffff000001f52600, ffff000001f526c0) [ 1.621570] [ 1.621579] The buggy address belongs to the physical page: [ 1.621593] page: refcount:1 mapcount:0 mapping:0000000000000000 index:0x0 pfn:0x81f52 [ 1.621618] flags: 0x0(zone=0) [ 1.621637] page_type: f5(slab) [ 1.621661] raw: 0000000000000000 ffff0000000013c0 dead000000000122 0000000000000000 [ 1.621678] raw: 0000000000000000 0000000080100010 00000001f5000000 0000000000000000 [ 1.621689] page dumped because: kasan: bad access detected [ 1.621699] [ 1.621705] Memory state around the buggy address: [ 1.621718] ffff000001f52580: 00 fc fc fc fc fc fc fc fc fc fc fc fc fc fc fc [ 1.621732] ffff000001f52600: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [ 1.621746] >ffff000001f52680: 00 00 00 00 00 00 00 00 fc fc fc fc fc fc fc fc [ 1.621756] ^ [ 1.621768] ffff000001f52700: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 [ 1.621782] ffff000001f52780: 00 00 00 00 00 00 00 00 fc fc fc fc fc fc fc fc [ 1.621793] ==================================================================