Other Parts Discussed in Thread: BQ28Z610, EV2400
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ28Z610 主题中讨论的其他器件: EV2400
工具/软件:
大家好、我遇到了 bq28z610 BMS 芯片问题。 它不会打开充电 FET、我找不到任何命令。
由于我没有 EV2400 USB 桥接器、因此我使用此 Arduino 草图阅读 BMS: https://github.com/asilichenko/bq28z610-arduino-driver
输出如下:
SS (Bit 11): SAFETY mode status: 1 SDV (Bit 10): SHUTDOWN triggered via low pack voltage: 0 SEC1 (Bit 9): 0 SEC0 (Bit 8): 1 BTP_INT (Bit 7): Battery Trip Point (BTP) Interrupt output: 1 CHG (Bit 2): CHG FET status: 0 DSG (Bit 1): DSG FET status: 1 === 12.2.27 AltManufacturerAccess() 0x0051 SafetyStatus 0000000000000000 0000000000000000 === 12.2.26 AltManufacturerAccess() 0x0050 SafetyAlert 0000000000100000 0000000000000000 === 12.1.1 0x00/01 ManufacturerAccess() Control: SEC1 (Bit 14): SECURITY Mode: 0 SEC0 (Bit 13): SECURITY Mode: 0 AUTHCALM (Bit 12): Automatic CALIBRATION mode: 0 CheckSumValid (Bit 9): Checksum Valid: 1 BTP_INT (Bit 7): Battery Trip Point Interrupt: 0 LDMD (Bit 3): LOAD Mode: 0 R_DIS (Bit 2): Resistance Updates: 1 VOK (Bit 1): Voltage OK for QMax Update: 0 QMax (Bit 0): QMax Updates. This bit toggles after every QMax update: 0 === 12.1.26 0x32/33 ChargingCurrent(): 0 mA === 12.1.25 0x30/31 ChargingVoltage(): 0.000 V === 12.1.10 0x12/13 FullChargeCapacity(): 3961 mAh === 12.1.27 0x3C/3D DesignCapacity(): 4400 mAh batteryStatus: 208 manufacturingStatus: 16 operationStatus: 18818 safetyStatus: 0 safetyAlert: 2097152 controlRegister: 516 chargingCurrent: 0 chargingVoltage: 0.00 fullChargeCapacity: 3961.00 designCapacity: 4400.00 DONE #####################
在读数中、表明电池已完全放电。 这对我来说毫无意义、因为电池处于中等充电电压。 此外、如果已放电、不应该启用充电?