This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ76952:在设置的时间间隔内未开启平衡

Guru**** 2540260 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1530508/bq76952-balancing-is-not-turnning-on-for-setted-time-interval

器件型号:BQ76952

工具/软件:

大家好、以下是我的设置配置、我已将平衡间隔时间设置为 5 秒、但每次仅在 500 毫秒内开启。请提供相关帮助。

BQ769x2_SetRegister (BalancingConfiguration、0x03、1);

BQ769x2_SetRegister (CellBalanceInterval、0x05、1);// Cell Balance Interval 5 秒
BQ769x2_SetRegister (CellBalanceMaxCells、0x01、1);// Cell Balance Max Cells 5

BQ769x2_SetRegister (CellBalanceMinCellVCharge、CombineConfigPacket.BMS0DetailsConfiguration.BalanceStartVoltage、2);//Cell Balance Min Cell V (Charge) 3200mV
BQ769x2_SetRegister (CellBalanceMinDeltaCharge、CombineConfigPacket.BMS0DetailsConfiguration.BalanceWindow、1);//电芯平衡最小差值(电荷)30mV
BQ769x2_SetRegister (CellBalanceStopDeltaCharge、(CombineConfigPacket.BMS0DetailsConfiguration.BalanceWindow - 10)、1);//Cell Balance Stop Delta (Charge) 20mV

BQ769x2_SetRegister (CellBalanceMinCellVRelax、CombineConfigPacket.BMS0DetailsConfiguration.BalanceStartVoltage、2);//电芯平衡最小电芯 V (Relax) 3200mV
BQ769x2_SetRegister (CellBalanceMinDeltaRelax、CombineConfigPacket.BMS0DetailsConfiguration.BalanceWindow、1);//Cell Balance Min Delta (Relax) 30mV
BQ769x2_SetRegister (CellBalanceStopDeltaRelax、(CombineConfigPacket.BMS0DetailsConfiguration.BalanceWindow - 10)、1);//Cell Balance Stop Delta (Relax) 15mV