This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS40170:使用低压降电压进行设计

Guru**** 2779905 points

Other Parts Discussed in Thread: TPS40170, LM25145

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1537178/tps40170-design-with-low-dropout-voltage

器件型号:TPS40170
主题中讨论的其他器件: LM25145

工具/软件:

您好、

请告诉我以下情况:

toff 数据表中列出的 TPS40170 (max) 是否是 toff (min) 的错误?

2.是否可以使用 TPS40170 设计 22.8Vin、22.0Vout、Fsw=100kHz?

由于占空比=96.5%、ton=9649ns、toff = 351ns、因此满足最短导通时间和最短关断时间条件。

此致、