请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ27Z746工具/软件:
尊敬的专家:
拔下充电器后、BQ27Z746 快速充电至 RSOC 80%、是否可以在不降低 RSOC 的情况下将 RSOC 保持 80% 4 小时?
Joyce
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.