This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TUSB1046A-DCI:TUSB1046A-DCIRNQR

Guru**** 2450590 points
Other Parts Discussed in Thread: BQ24610

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1533714/tusb1046a-dci-tusb1046a-dcirnqr

器件型号:TUSB1046A-DCI
主题:BQ24610 中讨论的其他器件

工具/软件:

麻煩幫我Review 附件線路圖 μ s。
Type-C交替模式转接驱动开关:TUSB1046A-DCIRNQR、设计功能:通过SoC提供独立的USB3.2 Gen和DP信号做Type μ F-C 交替模式应用 Ω
PD芯片:TPS25730D、设计功能:与Type C适配器协商20V、5A功能为本机电池充电和系统运行 Ω
充电器 IC:BQ24610、设计功能:为4串1并聚合物锂电池实现阶梯式充电、电池满充18V、相关电池信息和充电设置在线路图中有备注