请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPSM33615主题中讨论的其他器件: TPSM63602
工具/软件:
您好团队:
TPSM33615 是否可在以下条件下使用? 根据数据表、输出电压(TPSM33615 CAN 输出)高达 14V。
输入电压:18V~30V(典型值 24V)->输出电压:15V、1A

此致、
Shotaro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.