Other Parts Discussed in Thread: TPS92201A
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号: TPS92201A
现在、我正在使用 TPS92201A 进行设计、以驱动 4 个并联 LED(最大电流约为 80mA)。
如果我将 0.1uF 电容器与 4 个 LED 并联、是否存在任何问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.