This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 找到一个小封装,用于负功率,额定电流为3.3~5V 输入/-2V/600 mA

Guru**** 2810855 points

Other Parts Discussed in Thread: TPS62933

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1085323/finding-a-small-package-for-negative-power-with-3-3-5v-input--2v-600-ma-outpur-current-rating

“线程:TPS62933”中讨论的其它部件

是否有人建议使用小型封装来输出负功率

输入功率:2.5V ~ 5V

输出功率:至少-2V @ 600mA  

非常感谢。