This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS6.5217万:将PMIC从TPS6.591万A3更改为TPS6.5217万CRSLR

Guru**** 2589280 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1087289/tps65217-change-pmic-from-tps65910a3-to-tps65217crslr

部件号:TPS6.5217万

您好,

我有一个自定义主板,它一直在启动内核...

U-Boot 2020.01-00001-g5704c41f23-dirty (Mar 18 2022 - 19:02:07 +0800)

CPU : AM335X-GP rev 2.1
Model: TI AM335x Coupler(uboot)
DRAM: 512 MiB
WDT: Started with servicing (60s timeout)
NAND: 0 MiB
MMC: OMAP SD/MMC: 0
Loading Environment from FAT... *** Warning - bad CRC, using default environment

<ethaddr> not set. Validating first E-fuse MAC
Net: Could not get PHY for ethernet@4a100000: addr 0
eth0: ethernet@4a100000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4211200 bytes read in 286 ms (14 MiB/s)
40236 bytes read in 6 ms (6.4 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff3000, end 8ffffd2b ... OK

Starting kernel ...

我发现定制主板上的VDD_MPU为1.1V,但我希望它应该是1.26V,就像TI-EVMSK一样。(事实上,在AM335x-evmsk上测量后,它是1.31V)

这可能是导致我的主板cat无法进入内核的根本原因。

以下是修改AM335x-evmsk.dts的步骤,

1.将I2C从属ID从0x2D修改为0x24

2.修改TPS节点

// SPDX-License-Identifier: GPL-2.0-only
/*
 * Copyright (C) 2012 Texas Instruments Incorporated - http://www.ti.com/
 */

/*
 * AM335x Starter Kit
 * www.ti.com/.../tmdssk3358
 */

/dts-v1/;

#include "am33xx.dtsi"
#include <dt-bindings/pwm/pwm.h>
#include <dt-bindings/interrupt-controller/irq.h>

/ {
	model = "TI AM335x Coupler(kernel)";
	compatible = "ti,am335x-evmsk", "ti,am33xx";

	cpus {
		cpu@0 {
			cpu0-supply = <&dcdc2_reg>;
		};
	};

	memory@80000000 {
		device_type = "memory";
		reg = <0x80000000 0x20000000>; /* 512 MB */
	};

	chosen {
		stdout-path = &uart0;
	};

	v5d: fixedregulator0 {
		compatible = "regulator-fixed";
		regulator-name = "+5V";
		regulator-min-microvolt = <5000000>;
		regulator-max-microvolt = <5000000>;
		regulator-boot-on;
	};

	/* TLV62065DSGR */
	v1_0d_reg: fixedregulator-v1_0d {
		compatible = "regulator-fixed";
		regulator-name = "+1V0";
		vin-supply = <&v5d>;
		regulator-min-microvolt = <1000000>;
		regulator-max-microvolt = <1000000>;
	};

	/* TLV62065DSGR */
	v2_5d_reg: fixedregulator-v2_5d {
		compatible = "regulator-fixed";
		regulator-name = "+2V5";
		vin-supply = <&v5d>;
		regulator-min-microvolt = <2500000>;
		regulator-max-microvolt = <2500000>;
	};

	/* TLV62065DSGR */
	v3_3d_reg: fixedregulator-v3_3d {
		compatible = "regulator-fixed";
		regulator-name = "+3V3";
		vin-supply = <&v5d>;
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
	};

	leds {
		pinctrl-names = "default";
		pinctrl-0 = <&user_leds_s0>;

		compatible = "gpio-leds";

		led@1 {
			label = "LED RUN : Green";
			gpios = <&gpio2 0 GPIO_ACTIVE_LOW>;
			default-state = "off";
		};

		led@2 {
			label = "LED BF : Red";
			gpios = <&gpio1 29 GPIO_ACTIVE_LOW>;
			default-state = "off";
		};

		led@3 {
			label = "LED MS : Green";
			gpios = <&gpio2 3 GPIO_ACTIVE_LOW>;
			default-state = "off";
		};

		led@4 {
			label = "LED MS : Red";
			gpios = <&gpio2 4 GPIO_ACTIVE_LOW>;
			default-state = "off";
		};
		
		led@5 {
			label = "LED NS : Green";
			gpios = <&gpio2 5 GPIO_ACTIVE_LOW>;
			default-state = "off";
		};

		led@6 {
			label = "LED NS : Red";
			gpios = <&gpio2 2 GPIO_ACTIVE_LOW>;
			default-state = "off";
		};
	};
};

&am33xx_pinmux {
	pinctrl-names = "default";

	user_leds_s0: user_leds_s0 {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_GPMC_CSN3, PIN_OUTPUT_PULLDOWN, MUX_MODE7)	    /* GPMC_CSn3.gpio2_0 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_CSN0, PIN_OUTPUT_PULLDOWN, MUX_MODE7)	    /* GPMC_CSn0.gpio1_29 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_OEN_REN, PIN_OUTPUT_PULLDOWN, MUX_MODE7)	    /* GPMC_OEn_REn.gpio2_3 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_WEN, PIN_OUTPUT_PULLDOWN, MUX_MODE7)	        /* GPMC_WEn.gpio2_4 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_BEN0_CLE, PIN_OUTPUT_PULLDOWN, MUX_MODE7)	/* GPMC_BEn0_CLE.gpio2_5 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_ADVN_ALE, PIN_OUTPUT_PULLDOWN, MUX_MODE7)	/* GPMC_ADVn_ALE.gpio2_2 */
		>;
	};

	i2c0_pins: pinmux_i2c0_pins {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_I2C0_SDA, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_I2C0_SCL, PIN_INPUT_PULLUP, MUX_MODE0)
		>;
	};

	uart0_pins: pinmux_uart0_pins {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_UART0_RXD, PIN_INPUT_PULLUP, MUX_MODE0)      /* uart0_rxd.uart0_rxd */ /* 0x0970-0x0800=0x0170  */
			AM33XX_PADCONF(AM335X_PIN_UART0_TXD, PIN_OUTPUT_PULLDOWN, MUX_MODE0)   /* uart0_txd.uart0_txd */ /* 0x0974-0x0800=0x0174 */
		>;
	};

	cpsw_default: cpsw_default {
		pinctrl-single,pins = <
			/* Slave 1 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TX_EN, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* mii1_txen.rgmii1_tctl */
			AM33XX_PADCONF(AM335X_PIN_MII1_RX_DV, PIN_INPUT_PULLDOWN, MUX_MODE2)	/* mii1_rxdv.rgmii1_rctl */
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD3, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* mii1_txd3.rgmii1_td3 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD2, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* mii1_txd2.rgmii1_td2 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD1, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* mii1_txd1.rgmii1_td1 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD0, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* mii1_txd0.rgmii1_td0 */
			AM33XX_PADCONF(AM335X_PIN_MII1_TX_CLK, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* mii1_txclk.rgmii1_tclk */
			AM33XX_PADCONF(AM335X_PIN_MII1_RX_CLK, PIN_INPUT_PULLDOWN, MUX_MODE2)	/* mii1_rxclk.rgmii1_rclk */
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD3, PIN_INPUT_PULLDOWN, MUX_MODE2)	    /* mii1_rxd3.rgmii1_rd3 */
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD2, PIN_INPUT_PULLDOWN, MUX_MODE2)	    /* mii1_rxd2.rgmii1_rd2 */
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD1, PIN_INPUT_PULLDOWN, MUX_MODE2)	    /* mii1_rxd1.rgmii1_rd1 */
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD0, PIN_INPUT_PULLDOWN, MUX_MODE2)	    /* mii1_rxd0.rgmii1_rd0 */

			/* Slave 2 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A0, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a0.rgmii2_tctl */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A1, PIN_INPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a1.rgmii2_rctl */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A2, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a2.rgmii2_td3 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A3, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a3.rgmii2_td2 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A4, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a4.rgmii2_td1 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A5, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a5.rgmii2_td0 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A6, PIN_OUTPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a6.rgmii2_tclk */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A7, PIN_INPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a7.rgmii2_rclk */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A8, PIN_INPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a8.rgmii2_rd3 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A9, PIN_INPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a9.rgmii2_rd2 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A10, PIN_INPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a10.rgmii2_rd1 */
			AM33XX_PADCONF(AM335X_PIN_GPMC_A11, PIN_INPUT_PULLDOWN, MUX_MODE2)	/* gpmc_a11.rgmii2_rd0 */
		>;
	};

	cpsw_sleep: cpsw_sleep {
		pinctrl-single,pins = <
			/* Slave 1 reset value */
			AM33XX_PADCONF(AM335X_PIN_MII1_TX_EN, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_RX_DV, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD3, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD2, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD1, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_TXD0, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_TX_CLK, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_RX_CLK, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD3, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD2, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD1, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MII1_RXD0, PIN_INPUT_PULLDOWN, MUX_MODE7)

			/* Slave 2 reset value*/
			AM33XX_PADCONF(AM335X_PIN_GPMC_A0, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A1, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A2, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A3, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A4, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A5, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A6, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A7, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A8, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A9, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A10, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_GPMC_A11, PIN_INPUT_PULLDOWN, MUX_MODE7)
		>;
	};

	davinci_mdio_default: davinci_mdio_default {
		pinctrl-single,pins = <
			/* MDIO */
			AM33XX_PADCONF(AM335X_PIN_MDIO, PIN_INPUT_PULLUP | SLEWCTRL_FAST, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MDC, PIN_OUTPUT_PULLUP, MUX_MODE0)
		>;
	};

	davinci_mdio_sleep: davinci_mdio_sleep {
		pinctrl-single,pins = <
			/* MDIO reset value */
			AM33XX_PADCONF(AM335X_PIN_MDIO, PIN_INPUT_PULLDOWN, MUX_MODE7)
			AM33XX_PADCONF(AM335X_PIN_MDC, PIN_INPUT_PULLDOWN, MUX_MODE7)
		>;
	};

    /* SD Card */
	mmc1_pins: pinmux_mmc1_pins {
		pinctrl-single,pins = <
			AM33XX_PADCONF(AM335X_PIN_SPI0_CS1, PIN_INPUT, MUX_MODE7) 		/* spi0_cs1.gpio0_6 */
			AM33XX_PADCONF(AM335X_PIN_MMC0_DAT0, PIN_INPUT_PULLUP, MUX_MODE0)       /* mmc0_dat0.mmc0_dat0 */
			AM33XX_PADCONF(AM335X_PIN_MMC0_DAT1, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_DAT2, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_DAT3, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_CMD, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MMC0_CLK, PIN_INPUT_PULLUP, MUX_MODE0)
			AM33XX_PADCONF(AM335X_PIN_MCASP0_ACLKR, PIN_INPUT, MUX_MODE4)		/* mcasp0_aclkr.mmc0_sdwp */
		>;
	};
};

&uart0 {
	pinctrl-names = "default";
	pinctrl-0 = <&uart0_pins>;

	status = "okay";
};

&i2c0 {
	pinctrl-names = "default";
	pinctrl-0 = <&i2c0_pins>;

	status = "okay";
	clock-frequency = <400000>;

	tps: tps@24 {
		reg = <0x24>;
	};
};

&usb {
	status = "okay";
};

&usb_ctrl_mod {
	status = "okay";
};

&usb0_phy {
	status = "okay";
};

&usb0 {
	status = "okay";
};

&cppi41dma  {
	status = "okay";
};

#include "tps65217.dtsi"

&tps {
	regulators {
		dcdc1_reg: regulator@0 {
			regulator-name = "vdds_dpr";
			regulator-always-on;
		};

		dcdc2_reg: regulator@1 {
			regulator-name = "vdd_mpu";
			regulator-min-microvolt = <925000>;
			regulator-max-microvolt = <1351500>;
			regulator-boot-on;
			regulator-always-on;
		};

		dcdc3_reg: regulator@2 {
			regulator-name = "vdd_core";
			regulator-min-microvolt = <925000>;
			regulator-max-microvolt = <1150000>;
			regulator-boot-on;
			regulator-always-on;
		};

		ldo1_reg: regulator@3 {
			regulator-name = "vio,vrtc,vdds";
			regulator-always-on;
		};

		ldo2_reg: regulator@4 {
			regulator-name = "vdd_3v3aux";
			regulator-always-on;
		};

		ldo3_reg: regulator@5 {
			regulator-name = "vdd_1v8";
			regulator-always-on;
		};

		ldo4_reg: regulator@6 {
			regulator-name = "vdd_3v3a";
			regulator-always-on;
		};
	};
};

&mac {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&cpsw_default>;
	pinctrl-1 = <&cpsw_sleep>;
	status = "okay";
};

&davinci_mdio {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&davinci_mdio_default>;
	pinctrl-1 = <&davinci_mdio_sleep>;
	status = "okay";

	ethphy0: ethernet-phy@0 {
		reg = <0>;
	};

	ethphy1: ethernet-phy@1 {
		reg = <1>;
	};
};

&cpsw_emac0 {
	phy-handle = <&ethphy0>;
	phy-mode = "rgmii-id";
};

&cpsw_emac1 {
	phy-handle = <&ethphy1>;
	phy-mode = "rgmii-id";
};

/* SD Card */
&mmc1 {
	status = "okay";
	vmmc-supply = <&v3_3d_reg>;
	bus-width = <4>;
	pinctrl-names = "default";
	pinctrl-0 = <&mmc1_pins>;
	cd-gpios = <&gpio3 14 GPIO_ACTIVE_LOW>;
};

&sham {
	status = "okay";
};

&aes {
	status = "okay";
};

&gpio0 {
	ti,no-reset-on-init;
};

&rtc {
	status = "disabled";
};

是否有更多解决此问题的建议?