This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM5008:2.4GHz无线MCU电源设计。 LM5008与LMR1.6006万X

Guru**** 2452260 points
Other Parts Discussed in Thread: CC2541, LM5008

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/575389/lm5008-power-supply-design-for-2-4ghz-wireless-mcu-lm5008-vs-lmr16006x

部件号:LM5008
主题中讨论的其他部件:CC2541

您好,

我们正在设计48V至3.3V直流降压转换器,为我们的板载无线MCU (CC2541)供电。 感谢TI提供WEBENCH Designer -工具为我们节省了大量的IC选择和电路设计时间。

目前,我们无法在LM5008和LMR1.6006万X之间作出决定。

LM5008具有低切换频率213kHz和输出电压p-p 0.44mV。 但负载瞬态Vp-p为40mV

LMR1.6006万X 具有中等切换频率700kHz和输出电压p-p 1.01mV。 但是,负载瞬态Vp-p仅为8mV。

1)在WEBENCH中,显示"解决方案"表中的"可视化器"页面仅提到LM5008的输出p-p为0.44mV,而电气模拟页面图形显示稳态和负载瞬态下的40mV峰-峰。 那么,"可视化器"页表中提到的0.44mV输出p-p是什么? 不确定我们读取的图形是否正确。

2) TI或以前有电源设计经验的人员能否向我们推荐哪一种(即LM5008或LMR1.6006万X)更适合2.4GHz无线MCU (CC2541)?