This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ2.4617万:由于V LOWV=1.55V固定预充电至快速充电过渡阈值,因此,是bq2.4617万限制电池的低切断电压

Guru**** 2455000 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/574846/bq24617-is-bq24617-is-limiting-lower-cut-off-voltage-of-battery-due-to-v-lowv-1-55v-fixed-precharge-to-fast-charge-transition-threshold

部件号:BQ2.4617万

我正在使用bq2.4617万 IC为RRC2020电池组充电 ,该电池组允许将电池调节电压设置为13V。 现在,对于VFB针脚上设计的13V调节电压的电阻反馈,由于V LOWV (预充电到快速充电过渡阈值),蓄电池的低切断电压(我需要注意)大约为9.6V VFB引脚处为1.55V (固定),但实际蓄电池低切断电压为8.1V。

现在假设我把电池放电到8.5V并推入充电。 在这种情况下,如果VFB引脚电压在预充电时间(30分钟)内未超过V LOWV阈值 然后充电器将会声明故障。总的来说,由于V LOWV=1.55V固定在IC侧,而不允许用户外部设置,我将无法使用全部电池容量(100WH)。


请建议我一些克服上述限制的方法。