This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] WEBENCH®︎Tools/LM2674:Webench中的值与数据表计算中的值不匹配

Guru**** 2516170 points
Other Parts Discussed in Thread: LM2674

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/571742/webench-tools-lm2674-values-in-webench-don-t-match-values-in-datasheet-calculations

部件号:LM2674

工具/软件:WEBENCHRegistered设计工具

我正在使用LM2674开关调节器,在最大负载电流为.5A时,将输入电压从24至33V降至3.3V。 当我使用数据表第13页上的说明查找L1时,我转至第24页上的图24,使用最大输入电压= 33V,最大负载电流=.5A。 图中显示我应该使用L21,它是68 uh。 在Webench,他们说L1应该是100 uh (在数据表上是L20)。

同样,我找到了另一个答案:第14页显示了表2,无论我在Webench上使用我的68 uH还是100uH,我的Cout应该是100或120 UF,但Webench的Cout应该是47uF。 这些值非常不同,我找不到任何其他文件来模拟LM2674 (如LTSpice或Altium Design)来验证这些值。

我使用哪些值? 是否仍要返回检查这些值?

谢谢!