This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS6.103万:升压LED驱动器

Guru**** 2460850 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/571681/tps61030-boost-led-driver

部件号:TPS6.103万

您好,

 我想知道TPS6103x是否可以用作LED驱动器,在基本原理图中用1个或多个串联LED替换R3 ,并计算R4=0.5V/ILED。

典型示例为Vin=2.4V和Vout 3.5V (3V为1个LED指示灯降+0.5V为R4);ILED=0.6A

谢谢

Umberto