This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] BQ2.404万:使用BQ2.404万的充电电流限制

Guru**** 2536950 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/571330/bq24040-charge-current-limit-with-bq24040

部件号:BQ2.404万

您好,

我之前使用过BQ2.4055万充电器IC,但由于它最近已成为NRND,我将用非常相似的BQ2.404万替换它。 事实上,我只能注意到两者之间的两个差异: 快速电流编程电阻器的值范围,以及BQ2.404万上没有D+和D-引脚,BQ2.4055万中使用这些引脚来检测电源,以便不会使只能提供100mA的USB端口过载。

现在,这不是一个问题,不存在这种检测? 按照我所看到的方式,我必须用ISET电阻设置100mA的限值。

另外,如果没有D+/D-针脚,是否需要将此针脚从主机连接到USB电源连接器?

谢谢

Vítor Pereira