This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS6.0402万:高故障率

Guru**** 2693225 points

Other Parts Discussed in Thread: OPA4197

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/578790/tps60402-high-failure-rate

部件号:TPS6.0402万
主题中讨论的其他部件:OPA4197

我一直在多种设计中使用TPS6.0402万DBVR来明显地产生负轨。  到目前为止,他们都是完美无瑕的。  我看到输入,接地和输出的高故障率都在某种组合中短路(输入到接地,输出到接地,或在某些情况下全部三个短接在一起)。  

我正在研究的一款新产品需要+24V输入,并将其降至+5V。  然后,+5V与TPS6.0402万反转至-5V。  然后,+/-5V用于为四路运算放大器(OPA4197)供电。

调节器具有10uF输入盖和22uF输出盖。  TPS6.0402万具有1uF输入盖,3.3uF飞盖和3.3uF输出盖。  5V轨通过一个10欧姆电阻器,然后在运算放大器之前通过一个10nF电容。

这种方式我损失了将近20个充油泵,我无法找出原因。