This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LM5143-Q1EVM-2100:2100:EVM单输出双相同步降压配置

Guru**** 2553780 points
Other Parts Discussed in Thread: LM5143, LM5143-Q1, LM5117

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1094506/lm5143-q1evm-2100-evm-single-output-two-phase-sync-buck-configuration

部件号:LM5143-Q1EVM-2100</s>2100
主题中讨论的其他部件:LM5143LM5143-Q1LM5117

大家好,

我需要检查LM5143的双相交错性能。 您能否查看以下问题?

1.在EVM中填充LM5143-Q1。 您能否确认LM5143和LM5143-Q1将显示相同的性能?

2. EVM配置为双同步降压。 您能否确认将EVM配置为 单输出双相同步降压所需的修改?

(1) FB1/2:DNP R22,短R30

(2)模式:S2至VDDA

(3) SS1/2:DNP C51,简称S1B

(4) COMP1/2:DNP C52,C54和R33, 简称S1A

(5) VOUT1/2: 短R34

(6)还有事吗?