This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] UCC2.8056万:高电压时的调节问题

Guru**** 2539060 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1101259/ucc28056-regulation-issue-at-higher-voltage

部件号:UCC2.8056万
主题中讨论的其他部件:UCC2.878万

你(们)好

我使用的是用于60W交流-直流适配器的UCC2.8056万B版本  

这是我使用的电路原理图  

我在测试期间观察到的是,在180VAC至220VAC的特定电压范围内  

我的输入电流波形失真,直流总线未调节至377V  

请帮助解决此问题