请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TPS3847 TPS3847具有MR引脚。 VCC可以是12V,MR可以是3.3V吗? 问题在于低VCC为12V,因此3.3V的MR会导致内部缓冲处于线性模式,然后吸入过多电流。
此致
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.