This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS56.32万:是否可以输出电压=0.9V?

Guru**** 1828310 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1100882/tps563200-is-it-possible-vout-0-9v

部件号:TPS56.32万

你好,我是Jun

我要使用TPS56.32万DDCR,输出电压=0.9V

<详细条件>

1. VIN:9.6V~14.4V

输出电压:0.9V

3.负载电流:约2A

没问题吗?

请检查。

谢谢