请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5088 大家好、我想得到一些澄清。
LM5088数据表指示设计人员将引脚9 (OUT)连接到输出电压(Vout)。 Abs. max 表未指定引脚9的限值、因此默认值为7V。这是正确的吗? 因此 LM5088的最大输出电压为7V?
谢谢你。
-Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.