This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMR43610-Q1:请帮助推荐一些芯片

Guru**** 2782485 points

Other Parts Discussed in Thread: LMR43610, TLVM13620

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1109674/lmr43610-q1-please-help-recommend-some-chips

器件型号:LMR43610-Q1
主题中讨论的其他器件:LMR43610TLVM13620

我们需要电源转换芯片、输入电压范围为6Vdc ~ 18VDC、输出5V/1A、需要有使能端口、可以通过外部使能信号控制芯片是否正常工作、请帮助推荐一些芯片以满足这些需求、谢谢!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    LMR43610可能是一个不错的解决方案。

    此外、TLVM13620