请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25672 您好、先生、
BQ25672 用于为两节电池充电、充电电流设置为2A、充电约半小时后、通过红外温度计测量的 BQ25672的温度接近60摄氏度、温度是正常还是太热?
宝黄
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.