请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5145 主题中讨论的其他器件: LM5143-Q1
你(们)好
您能否帮助检查 LM5145是否是12V 至0.85V/35A 应用的理想选择?
WEBENCH 显示其最大负载电流仅为20A、产品文件夹显示其最大负载电流为30A、两者均小于35A 要求


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.