请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM2673 数据表建议 Iadj > 1A。 但我们使用37.4K、1%电阻器配置了0.99A。 您能不能指定预期会出现什么问题、也可以使用0.99A。 最大平均负载电流为0.4A。 输入电压调节为15V、输出电压为12V。 电感为33uH。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.