请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS53321 您好!
我检查了数据表、器件支持的输入电压范围为4.5~18V。
我的客户设计的输出电压= 1.8V、输入电压= 4.5V 对于该设计来说是可以的、对吧?
另一个问题是器件具有最大占空比规格?
例如、如果输出电压设计为5V、则最小输入电压要求是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.