This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS53319:是否有任何方法可通过直流/直流转换器或模块将-12V 转换为-7V、-6A?

Guru**** 2504735 points
Other Parts Discussed in Thread: TPS5430, LMZM33604

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1064356/tps53319-is-there-any-method-to-convert--12v-to--7v--6a-by-a-dc-dc-converter-or-module

器件型号:TPS53319
主题中讨论的其他器件:TPS5430LMZM33604

在我的系统中、 只有两个输入电源轨: +12V、20A 和-12V、-20A (它们来自隔离式直流/直流砖型模块)。

现在、我想使用-7V、-6A 电压为功率放大器供电、我可以将其从-12V 电压转换吗? 如何实现?