请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPSM63606 大家好、团队、
我对 TPSM63606封装概述有疑问。
- 根据封装外形、0.5mm 间距引脚(引脚#2~ 7和#10~ 15)是否与中心稍微偏离?
- 您能告诉我引脚1 (#16)和引脚8 (#9)的尺寸吗?
引脚8和引脚7之间有尺寸、引脚2和引脚1之间有尺寸、但也想知道从封装边沿到引脚8和引脚1之间的尺寸。
此致、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.