请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS63000 您好!
根据数据表、TPS63000输出范围为1.2V~5.5V。
目前、我使用外部电阻分压器将其输出设置为1.2V、如下所示。
由于这是该稳压器的最小值、我确定是否存在任何问题。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.