请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPSM831D31 您好、先生、
VoutA+LOAD A (0.6V~1.3V、120A)的最大总电容值是多少?
VoutB+LOAD B 的最大总电容值是多少(0.35V~1.3V、40A)?
恐怕总电容太大、无法损坏 TPSM831D31。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、先生、
VoutA+LOAD A (0.6V~1.3V、120A)的最大总电容值是多少?
VoutB+LOAD B 的最大总电容值是多少(0.35V~1.3V、40A)?
恐怕总电容太大、无法损坏 TPSM831D31。