请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP5890 尊敬的团队:
我们是否有任何交流/直流解决方案可满足以下各项规格?
- VIN=120Vac、 Vo=16S1P、大约144V。 ˙7~8W 、PWM 调光
- VIN=18Vdc、RGB LED 驱动器(5S)、 R PWM 调光。 G PWM 调光、B PWM 调光:总功率7W
非常感谢!
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.