This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [参考译文] [常见问题解答] TPS549D22:TPS549B22/TPS549D22中的 PMBus 电路是否支持1.8V 上拉终端电压?

Guru**** 2502205 points
Other Parts Discussed in Thread: TPS549B22, TPS549D22

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1044467/faq-tps549d22-can-the-pmbus-circuits-in-the-tps549b22-tps549d22-support-1-8v-pull-up-termination-voltage

器件型号:TPS549D22
主题中讨论的其他器件:TPS549B22

问题:

TPS549B22和 TPS549D22上的 PMBus 引脚能否为上拉电阻器提供1.8V I/O 终端电压?

答案:

TPS549B22和 TPS549D22的 PMBus 引脚旨在满足 SMBus 3.1"高功率"1MHz 类电压和时序要求。

这包括1.35V 的输入电压"高电平"(VOH)最大线程保持和0.8V 的输入电压"低电平"(VIL)最小值、以支持1.8V 终端电压和0.4V 的最大输出电压低电平(VOL)(具有20mA 上拉电流)。

上拉端接电阻的大小应确保0.4V 输出端接电流小于20mA (不小于70Ω Ω)、同时确保在所用总线速度和总线电容的时序限制范围内有足够短的上升时间从0V 上升到1.35V。