请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS92692-Q1 大家好、
您能否按 如下方式估算8~16V 输入电压和 LED 条件下的近似转换效率曲线(PI/Po):
- LED 恒定电流1.2A±0.1A
(1) LED 电压为12V
(2) LED 电压为8V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、
您能否按 如下方式估算8~16V 输入电压和 LED 条件下的近似转换效率曲线(PI/Po):
(1) LED 电压为12V
(2) LED 电压为8V