请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMR12010 我对 LMR12010电路的设计有疑问、
附件是使用 WEBENCH设计器获得的建议电路,
升压引脚需要添加一个5V 电池并将二极管串联。
Vout 能否串联一个二极管、然后像数据表图15中所示那样返回到升压引脚?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.